Hi,
For one of the project we wanted to support blend de-interlace to capture camera content and do scaling and color conversion.
Platform details - Linux 4.14.98-2.3.2 running on imx8qx
Is blend deinterlace supported as part of 4.14.98-2.3.2?
As part of the function mxc_isi_channel_set_deinterlace, we could see the blend de-interlace method is marked as TODO.
/* de-interlacing method
* Weaving-------------Yes
* Line Doubling-------No
* Blending -----------TODO*/
Can we get few details on configuring blend de-interlace mode?
Based on linux reference implementation we are doing it on M4. As per the Application processor reference manual (IMX8DQXPRM_Rev_D.pdf), we tried configuring the ISI channels, but we could not succeed. Looks like 'source from memory' for ISI0 is not functional
Here are the steps we followed
IS 0x5 the right value to be configured as SRC for ISI0? Do we need to do any specific configuration for input port 5?
In order to check for ISI0 configurations, ISI0 SRC field changed to 0x04, we could see the data present on input port 4, is this confirms the ISI0 configuration is correct?
As per this looks to be source from memory for ISI0 is not functional, any specific configurations needed other than input/output BUF configurations?
Do we need to do any trigger in case of blend de-interlace configuration? We have also tried software controlled memory read by configuring ISI4 for capture and weaving.
Thanks
Arun
Hi @igorpadykov,
Could you confirm that de-interlacing using blending is supported on the i.MX8QM too, when capturing interlaced signals from the MIPI-CSI? It’s because we got everything working so far (for PAL and NTSC), but it seems that the odd/even field indication is lost between the MIPI and ISI, or at least it looks like that. Basically, in 50% of the cases when a video signals is hooked up, it is getting properly de-interlaced, in the other cases the odd and even lines are swapped and things look ugly. It’s also unclear to us how the odd/even field indication gets transferred over the internal pixel link from the MIPI-CSI towards the ISI?
For your information, the odd/even lines getting swapped is already visible in the intermediate YUYV buffers generate by ISI channel 1, which then enters ISI channel 0 to get blended and CSC’ed.
Thanks in advance!
Regards.