I'm trying to make image "core-image-base" using bitbake for freescale imx6 platform. Things were working very well. I made image two times as well. But suddently it stopped working. I've used "bitbake core-image-base" command for making build.
below is the error I get. Could someone help me, what must have gone wrong?
'
| make: Leaving directory `/home/ramprasad/fsl-release-bsp-2/build-7/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.10.17-r0/image/usr/src/kernel'
| NOTE: make -j 4 imx6q-sabresd.dtb
| CC scripts/mod/devicetable-offsets.s
| GEN scripts/mod/devicetable-offsets.h
| HOSTCC scripts/mod/file2alias.o
| HOSTLD scripts/mod/modpost
| make[1]: `arch/arm/boot/dts/imx6q-sabresd.dtb' is up to date.
| NOTE: make -j 4 imx6q-sabresd-ldo.dtb
| CC scripts/mod/devicetable-offsets.s
| GEN scripts/mod/devicetable-offsets.h
| HOSTCC scripts/mod/file2alias.o
| HOSTLD scripts/mod/modpost
| make[1]: `arch/arm/boot/dts/imx6q-sabresd-ldo.dtb' is up to date.
| NOTE: make -j 4 imx6q-sabresd-hdcp.dtb
| CC scripts/mod/devicetable-offsets.s
| GEN scripts/mod/devicetable-offsets.h
| HOSTCC scripts/mod/file2alias.o
| HOSTLD scripts/mod/modpost
| make[1]: `arch/arm/boot/dts/imx6q-sabresd-hdcp.dtb' is up to date.
| NOTE: make -j 4 imx6q-sabresd-enetirq.dtb
| CC scripts/mod/devicetable-offsets.s
| GEN scripts/mod/devicetable-offsets.h
| HOSTCC scripts/mod/file2alias.o
| HOSTLD scripts/mod/modpost
| make[1]: *** No rule to make target `arch/arm/boot/dts/imx6q-sabresd- enetirq.dtb'. Stop.
make: *** [imx6q-sabresd-enetirq.dtb] Error 2
ERROR: oe_runmake failed
WARNING: exit code 1 from a shell command.
ERROR: Function failed: do_install (log file is located at /home/ramprasad/fsl-release-bsp-2/build-7/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.10.17-r0/temp/log.do_install.11111)
ERROR: Task 68 (/home/ramprasad/fsl-release-bsp-2/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.10.17.bb, do_install) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3610 tasks of which 3609 didn't need to be rerun and 1 failed.
No currently running tasks (1718 of 3640)
Summary: 1 task failed:
/home/ramprasad/fsl-release-bsp-2/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.10.17.bb, do_install
Summary: There was 1 ERROR message shown, returning a non-zero exit code
解決済! 解決策の投稿を見る。
That didn't help.
I did little more debugging to see what could be. Then I compared the sources directory with the backup I've a while ago. I see below lines changed:
File @ meta-fsl-arm/conf/machine/imx6qsabresd.conf has changes :
Back-up of source:
KERNEL_DEVICETREE = "imx6q-sabresd.dtb imx6q-sabresd-ldo.dtb imx6q-sabresd-hdcp.dtb"
Current file:
KERNEL_DEVICETREE = "imx6q-sabresd.dtb imx6q-sabresd-ldo.dtb imx6q-sabresd-hdcp.dtb imx6q-sabresd-enetirq.dtb imx6q-sabresd-uart.dtb"
KERNEL_IMAGETYPE = "zImage"
Then I removed "imx6q-sabresd-enetirq.dtb imx6q-sabresd-uart.dtb" and also KERNEL_IMAGETYPE = "zImage" , from meta-fsl-arm/conf/machine/imx6qsabresd.conf , then it all worked fine.
But I've not changed them, neither I did "repo sync". Any idea, how would these change?
I figured out answer for above problem. I needed to use "dhcp-client" instead of dhcp.
Only puzzling thing is, how did my "imx6qsabresd.conf" changed on it's own.
Now the problem in this thread is resolved. So I will be marking it as "Answered"
Hello Ramprasad,
If it was running correctly and no changes were made perhaps it would help to make a cleanall.
bitbake -c cleanall <IMAGE>
That didn't help.
I did little more debugging to see what could be. Then I compared the sources directory with the backup I've a while ago. I see below lines changed:
File @ meta-fsl-arm/conf/machine/imx6qsabresd.conf has changes :
Back-up of source:
KERNEL_DEVICETREE = "imx6q-sabresd.dtb imx6q-sabresd-ldo.dtb imx6q-sabresd-hdcp.dtb"
Current file:
KERNEL_DEVICETREE = "imx6q-sabresd.dtb imx6q-sabresd-ldo.dtb imx6q-sabresd-hdcp.dtb imx6q-sabresd-enetirq.dtb imx6q-sabresd-uart.dtb"
KERNEL_IMAGETYPE = "zImage"
Then I removed "imx6q-sabresd-enetirq.dtb imx6q-sabresd-uart.dtb" and also KERNEL_IMAGETYPE = "zImage" , from meta-fsl-arm/conf/machine/imx6qsabresd.conf , then it all worked fine.
But I've not changed them, neither I did "repo sync". Any idea, how would these change?
After, I pass through above step, I wanted to include dhcp. But I get below error. Any idea how can this be resolved?
ERROR: dhcp not found in the base feeds (imx6qsabresd cortexa9hf-vfp-neon-mx6 cortexa9hf-vfp-neon cortexa9hf-vfp armv7ahf-vfp-neon armv7ahf-vfp armv6hf-vfp armv5ehf-vfp armv5hf-vfp noarch any all).