BT.709 format in i.MX 6Dual.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BT.709 format in i.MX 6Dual.

Jump to solution
966 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Is it possible to support the output of BT.709 format in i.MX 6Dual.

(BT.709 looks like a BT.1120 with HSYNC、VSYNC、Field SYNC)

Best Regards,

Keita

Labels (4)
0 Kudos
1 Solution
741 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes in theory i.MX6 IPU hardware can support it, since it can output B1120

and it complies with BT709, from ITU-R BT.1120 sect.1.1 Coding characteristics:

The signals to be digitized should comply with the characteristics described in

Recommendation ITU-R BT.709, Part 1.

https://www.itu.int/dms_pubrec/itu-r/rec/bt/R-REC-BT.1120-4-200305-S!!PDF-E.pdf

Freescale provided community patch where HSYNC、VSYNC are already available

on pads:

Patch to Support BT656 and BT1120 Output For i.MX6 BSP

IPU1_DI0_PIN2 connected to adv7391 HSYNC pin. (option)

IPU1_DI0_PIN4 connected to adv7391 VSYNC pin. (option)

For "Field SYNC" signal seems IPU microcode should be modified,

I think you can request this from author on link above.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
742 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes in theory i.MX6 IPU hardware can support it, since it can output B1120

and it complies with BT709, from ITU-R BT.1120 sect.1.1 Coding characteristics:

The signals to be digitized should comply with the characteristics described in

Recommendation ITU-R BT.709, Part 1.

https://www.itu.int/dms_pubrec/itu-r/rec/bt/R-REC-BT.1120-4-200305-S!!PDF-E.pdf

Freescale provided community patch where HSYNC、VSYNC are already available

on pads:

Patch to Support BT656 and BT1120 Output For i.MX6 BSP

IPU1_DI0_PIN2 connected to adv7391 HSYNC pin. (option)

IPU1_DI0_PIN4 connected to adv7391 VSYNC pin. (option)

For "Field SYNC" signal seems IPU microcode should be modified,

I think you can request this from author on link above.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos