Audio codec not working with L4.1.15_1.1.0_ga_images

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Audio codec not working with L4.1.15_1.1.0_ga_images

689 次查看
sourabhdas
Contributor III

Hi,

I am using imx6ulevk board. I am new in audio codec stuff. Initially I tried with L3.14.38 prebuilt images that I downloaded from the nxp website.

I recorded some sound with arecord utility and played it back to my PC. It was playing well.

Next I tried with L4.1.15_1.1.0_ga_images which was the latest image that I downloaded from nxp website. I tried the arecord utility to record some sound, but it was not geting record. I tried this several times with L4.1.15_1.1.0_ga_images, but I am not able to record anything.

I tried this command:

arecord -d 10 test.wav

Kindly help me in this.

标签 (1)
标记 (1)
0 项奖励
2 回复数

523 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sourabh

please try procedure given in sect.7.3.5 Audio recording

attached Linux Guide and sect.28.2.4 Sound Card Information

Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

523 次查看
sourabhdas
Contributor III

Hi igor,

Thanks for your reply. I have gone through the Linux Reference Manual and got some brief idea about what all the drivers (like wm8960.c, imx-wm8960.c, fsl_sai.c) are doing.

I checked the drivers by putting some debug prints. They were loaded properly. So, what should I do next?

0 项奖励