Hello,
Measuring the MCLK driven by i.MX6 Solo out of GPIO_0 (muxed as CCM_CLKO1) reveals very poor clock quality. Although the NVCC_GPIO rail is at 3.3V, the MCLK only reaches 2V maximum and resembles more a triangular wave.
The register value of IOMUX_SW_PAD_CTL_PAD (address 0x20E05DC) is 0x130B0.
For comparison, both BCLK and LRCLK are nominal at 3.3V as expected and are square waveforms.
Please advise. Must register settings be changed? Perhaps the GPIO_0 can't drive hard enough?
Thank you,
Mikael
解決済! 解決策の投稿を見る。
Hi Mikael
yes reason may be insufficient drive strength/high capacitive load or very high
output frequency. Value " 0x130B0" corresponds to IOMUXC_SW_PAD_CTL_PAD_GPIO00
described in sect.37.4.371 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_GPIO00)
i.MX 6Solo/6DualLite Applications Processor Reference Manual
and one can try to set to max. values DSE, SPEED, SRE parameters.
May be recommended to use additional buffer as in i.MX6Q Sabre SD schematic spf-27392 p.8
Best regards
igor
Hi Mikael
yes reason may be insufficient drive strength/high capacitive load or very high
output frequency. Value " 0x130B0" corresponds to IOMUXC_SW_PAD_CTL_PAD_GPIO00
described in sect.37.4.371 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_GPIO00)
i.MX 6Solo/6DualLite Applications Processor Reference Manual
and one can try to set to max. values DSE, SPEED, SRE parameters.
May be recommended to use additional buffer as in i.MX6Q Sabre SD schematic spf-27392 p.8
Best regards
igor