Argon imx6ul SOM hang issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Argon imx6ul SOM hang issue

598件の閲覧回数
hardikbehere
Contributor I

We are facing following issue “argon imx6ul” SOM .

SOM gets hang if Ethernet is disable in device tree and menu config.

But if we connect pen-drive in same image (with disabled Ethernet in device tree) , then we are not facing SOM hang issue.

we are using kernel version 4.1.15-1.2.0+g77f6154.

ラベル(1)
タグ(1)
0 件の賞賛
1 返信

528件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi hardik

to check if this is specifc for that board, please try to reproduce issue

on nxp i.MX6UL EVK reference board with official nxp releases described on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

one can check using core-image-minimal image described in

Table 1. Freescale Yocto project images attached Yocto Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛