Are there any i.MX6/7/8 processors available in non-ROHS BGAs?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there any i.MX6/7/8 processors available in non-ROHS BGAs?

584 Views
emagii
Contributor II

For harsh environments you can get an exemption from the ROHS directive.

It is possible to reball to leaded balls, but it is very expensive.

Tags (1)
0 Kudos
2 Replies

524 Views
emagii
Contributor II

We have an exemption from the RoHS directive, and I know that we can reball,
and I know that it is expensive.

What I do not know is if NXP can deliver any iMX6 processors in leaded BGAs.

So I repeat the question:

  • Does NXP have any iMX6 or later application processors in leaded BGAs?
0 Kudos

524 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ulf Samuelsson,

Reballing the BGA’s yourself may be the more plausible option as there are no leaded i.MX part numbers being produced. You could always contact NXP sales to see if it would be possible to get a custom part, but it would depend a lot on whether the leaded processes are still available and the volume of parts you need.

I’ve heard of cases in which leaded flux is applied to the BGA but it’s not the ideal scenario in terms of mechanical reliability and it would require to be careful as the footprint wouldn’t be planned to accommodate the extra flux.

My apologies for the inconvenience!

Regards,

0 Kudos