Are there IBIS models for the i.MX6 Solo Lite USB pins?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are there IBIS models for the i.MX6 Solo Lite USB pins?

989件の閲覧回数
davidlindley
Contributor I

I have designed in the i.MX6 Solo Lite in my board.  I need to run SI sims on the USB traces.  I have downloaded the IBIS file, mx6sl_416mapbga13x13_autmtv, from Freescale.  I don't think the IBIS file implements a model for the USB pins.  It looks like the models for the USB D+/D- pins are listed as "NC".  Am I reading that correct?

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

680件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi David

yes, you are right, not all i.MX6 ibis models have usb,

for example i.MX6SDL has

IMX6_DL_S_IBIS : i.MX 6DualLIte and i.MX 6Solo IBIS File.

Probably you can use it. In general it is sufficient

to follow usb layuout guidelines in below document

IMX6SLHDG

Hardware Development Guide for i.MX 6SoloLite - User Guide

Best regards

chip

0 件の賞賛
返信