Hi All,
I am developping a commercial system using iMX51 + Qt 4.7.3 + simplegl driver.
The application uses opengl 32 bits. System has 256 MB of RAM used with the following bootloader prms:
gpu_memory=128M gpu_nommu
The application (called APP) is using opengl only in for 2 animation involving crossfading, bluring and brightness.
The vertex and fragment shader are very simple and are written inside 2 qml files.
Sometimes the application stucks with the following output:
APP: /u/build/nightly_build/build/ltib/rpm/BUILD/amd-gpu-src-11.05.01/driver/build/linux/mx51/../../../es20/src/gl2_framebufferobject.c:388: set_framebuffer: Assertion `0' failed.
I dont know the reason why. Does anybody know what is the meaning of this message?
Have you experienced this issue?
Any support is very appreciated. Thx.
Antonino, this DI will be closed if no response from your in 3 days.
Thanks,
Yixing
Antonino, FSL engineer is working on your questions now and needs your answer for further investigation. Please respnd as soon as possible.
Thanks,
Yixing
Do you only see issue when using a QT based application ?
regards,
Andre