Android5.1.1 on IMX6Q and IMX6DL debug console uart RX can't recevie data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android5.1.1 on IMX6Q and IMX6DL debug console uart RX can't recevie data

ソリューションへジャンプ
1,382件の閲覧回数
yangguang
Contributor II

I use mfgtools downlode android5.1.1 to freecale official imx6q development board,debug console use uart1(ttymxc0) ,when I started the development board ,I found the development board uart1 tx is ok,but rx can't work normal.Details as follows, i use pc serial tools connect the development board ,start the development board,when it enter uboot,i enter pc keyboard  any buttons ,the uboot command line can recive the data,this can prove uart hardware is good,when the development board enter the android systerm,,i enter pc keyboard  any buttons,the linux kernel command line can't recive the data.I want use the kernel command line test something,but why the uart rx isn't ok?

ラベル(4)
0 件の賞賛
返信
1 解決策
782件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

This is  a question of android which can be found in http://source.android.com/devices/tech/security/selinux/ and https://source.android.com/devices/tech/security/verifiedboot/index.html, but NXP still give answer in the user guide.

Android_User's_Guide.pdf

Untitled.png

Android_Quick_Start_Guide.pdf

Untitled.png

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
783件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

This is  a question of android which can be found in http://source.android.com/devices/tech/security/selinux/ and https://source.android.com/devices/tech/security/verifiedboot/index.html, but NXP still give answer in the user guide.

Android_User's_Guide.pdf

Untitled.png

Android_Quick_Start_Guide.pdf

Untitled.png

0 件の賞賛
返信
782件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the ADB ; refer to sections 3 (How do I use ADB over Ethernet?) 
and 4 (How do I set up a computer to support ADB?) of "Android_Frequently_Asked_Questions.pdf"

from NXP Android documentation.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信