from these directions http://reviews.androids.name/2011/03/i-mx-android-firmware-developers-manual-very-good/ I followed steps
3.2.1
3.2.3
3.2.5
for the imx51 bbg. The board I am using is the imx51 evk, which might be the issue but I am unsure. Just to be clear on exactly what I did:
I used fdisk to partition an sd card like this:
Partition Type/Index | Name | Start Offset | Size | File System | Content |
N/A | BOOT | 0 | 10 MB | N/A | bootloader/kernel/uramdisk images |
Primary 1 | MEDIA | 11 MB | User Defined | VFAT. Mount as /sdcards | Media file storage |
Primary 2 | SYSTEM | follow MEDIA | >= 200 MB | EXT4. Mount as /system (with read only) | Android system bin/libs (system.img) |
Logic 5 (Extended 3) | DATA | follow SYSTEM | > 200 MB | EXT4. Mount as /data | Android data (e.g. installed app) |
Logic 6 (Extended 3) | CACHE | follow DATA | > 10 MB | EXT4. Mount as /cache | Android cache |
Primary 4 | RECOVERY | follow CACHE | > 20 MB | EXT4. Mount as / in recovery mode | Root file system for recovery mode (recovery.img) |
Then I ran these commands
# mkfs.vfat /dev/sdx1
# mkfs.ext4 /dev/sdx2 -O ^extent -L system
# mkfs.ext4 /dev/sdx4 -O ^extent -L recovery
# mkfs.ext4 /dev/sdx5 -O ^extent -L data
# mkfs.ext4 /dev/sdx6 -O ^extent -L cache
# sudo dd if=u-boot-no-padding.bin of=/dev/sdx bs=1K seek=1; sync
# sudo dd if=uImage of=/dev/sdx bs=1M seek=1; sync
# sudo dd if=uramdisk.img of=/dev/sdx bs=1M seek=6; sync
Then I put the sd card into the imx51 and powered up the board (dip switch set all off except 7 and 8). UBoot loaded and I changed the environment variables to
bootdelay=1
baudrate=115200
netdev=eth0
ethprime=FEC0
uboot_addr=0xa0000000
kernel=uImage
nfsroot=/opt/eldk/arm
bootargs_base=setenv bootargs console=ttymxc0,115200 gpu_memory=16M
bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm
prg_uboot=tftpboot ${loadaddr} ${uboot}; protect off ${uboot_addr} 0xa003ffff; erase ${uboot_addr} 0xa003ffff; cp.b ${loadaddr} ${uboot_addr} ${filesize}; setenv filesize; saveenv
bootcmd_SD=run bootargs_base bootargs_android;mmc read 0 ${loadaddr} 0x800 1800;mmc read 0 ${rd_loadaddr} 0x2000 0x258;bootm ${loadaddr} ${rd_loadaddr}
bootargs_android=setenv bootargs ${bootargs} androidboot.console=ttymxc0 init=/init di1_primary calibration
bootcmd_android_recovery=run bootargs_base bootargs_android_recovery;mmc read 0 ${loadaddr} 0x800 0x1800;bootm
bootargs_android_recovery=setenv bootargs ${bootargs} init=/init root=/dev/mmcblk0p4 rootfs=ext4 di1_primary
ethact=FEC0
ethaddr=00:04:9f:00:ea:d3
fec_addr=00:04:9f:00:ea:d3
bootcmd=run bootcmd_SD; bootm ${loadaddr} 0x800 0x2000; mmc read 0 ${rd_loadaddr} 0x3000 0x300;
uboot=u-boot-no-padding.bin
bootargs=console=ttymxc0,115200 gpu_memory=16M androidboot.console=ttymxc0 init=/init di1_primary calibration
stdin=serial
stdout=serial
stderr=serial
loadaddr=0x90800000
rd_loadaddr=0x90B00000
And I get this error when I try to boot
BBG U-Boot > bootd
MMC read: dev # 0, block # 2048,count 6144 ...
6144 blocks read: OK
MMC read: dev # 0, block # 8192,count 600 ...
600 blocks read: OK
## Booting kernel from Legacy Image at 90800000 ...
Image Name: Linux-2.6.35.3-00026-g37d9315
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3150972 Bytes = 3 MB
Load Address: 90008000
Entry Point: 90008000
Verifying Checksum ... OK
Wrong Ramdisk Image Format
Ramdisk image is corrupt or invalid
## Booting kernel from Legacy Image at 90800000 ...
Bad Header Checksum
ERROR: can't get kernel image!
MMC read: dev # 0, block # 12288,count 768 ...
768 blocks read: OK
I am unfamiliar with UBoot / Android / Linux so I am expecting it to be a simple mistake. Let me know if you need anything else to diagnose why it won't boot the image.
Thanks
You're right.
You are using parameters for using WVGA. But you're using DVI instead.
Pleae, use this:
console=ttymxc0 init=/init androidboot.console=ttymxc0 di0_primary gpu_nommu, gpu_memory=32M video=mxcdi0fb:RGB24,1024x768M@60
di0_primary is for DVI
video=mxcdi0fb:RGB24,1024x768M@60 is the resolution and color.
Please, take a look on release notes to further info.
this appears to work however I am not getting any output on my dvi monitor. This is the last chunk of output that i have.
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
EXT4-fs (mmcblk0p5): recovery complete
EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: (null)
EXT4-fs (mmcblk0p6): recovery complete
EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: (null)
usb 2-1.6: new high speed USB device using fsl-ehci and address 3
scsi0 : usb-storage 2-1.6:1.0
scsi 0:0:0:0: Direct-Access USB TO I DE/SATA Device 0009 PQ: 0 ANSI: 0
sd 0:0:0:0: [sda] Attached SCSI disk
usb wakeup is here
otg udc wakeup
android_usb gadget: high speed config #1: android
I used to configure uboot this way:
U-Boot > setenv loadaddr 0x90800000
U-Boot > setenv rd_loadaddr 0x90D00000
U-Boot > setenv bootcmd 'run bootcmd_SD; bootm ${loadaddr} ${rd_loadaddr}'
U-Boot > setenv bootcmd_SD 'mmc read 0 ${loadaddr} 0x800 0x2000; mmc read 0 ${rd_loadaddr} 0x3000 0x300;'