Hi,
I am porting android lollipop 5.0 to sabre sd board. My android file system is not mounting i am facing the binder issue. even i tried with both 4GB and 8GB sd card also facing the same issue. Tried with prebuilt images also getting the same problem. Please guide me to resolve this issue.
I am getting the below log
EXT4-fs (dm-0): mounted filesystem with ordered data mode. Opts: barrier=1
fs_mgr: __mount(source=/dev/block/dm-0,target=/system,type=ext4)=0
fs_mgr: __mount(source=/dev/block/mmcblk2p4,target=/data,type=ext4)=-1
fs_mgr: fs_mgr_mount_all(): possibly an encryptable blkdev /dev/block/mmcblk2p4 for mount /data type ext4 )
fs_mgr: __mount(source=/dev/block/mmcblk2p6,target=/cache,type=ext4)=-1
fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk2p6 at /cache options: nomblk_io_submit error: Read-only file system
EXT4-fs (mmcblk2p7): INFO: recovery required on readonly filesystem
EXT4-fs (mmcblk2p7): write access unavailable, cannot proceed
fs_mgr: __mount(source=/dev/block/mmcblk2p7,target=/device,type=ext4)=-1
fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk2p7 at /device options: (null) error: Invalid argument
init: fs_mgr_mount_all returned an error
init: fs_mgr_mount_all returned unexpected error 255
SELinux: Could not set context for /cache: Read-only file system
rfkill: BT RF going to : off
binder: 154:154 transaction failed 29189, size 0-0
init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead
init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead
init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
android_usb: already disabled
mtp_bind_config
healthd: BatteryTemperaturePath not found
healthd: BatteryTechnologyPath not found
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
Thanks & Regards,
pushpa teja.c
Hi Pushpa,
Hoping you have not solved the issue,
Please check the partitioning of your SD card. That should solve binder issue. If you have solved then you may ignore or post your solution. It will help others.
Regards,
Manju
Hi SergioSolis,
Yes still i am facing the same issue with the demo images also. I did changes in fstab.freescale file to build the images for SD card booting rather than that i dint did any thing the fallowing change i did .
/devices/soc0/soc.1/2100000.aips-bus/2198000.usdhc/mmc_host /mnt/media_rw/extsd vfat defaults voldmanaged=sdcard:auto
/devices/soc0/soc.1/2100000.aips-bus/2184000.usb/ci_hdrc.0 /mnt/media_rw/udisk vfat defaults voldmanaged=sdcard:auto
/dev/block/mmcblk3p5 /system ext4 rw,barrier=1 wait,verify
/dev/block/mmcblk3p4 /data ext4 nosuid,nodev,nodiratime,noatime,nomblk_io_submit,noauto_da_alloc,errors=panic wait,encryptable=/dev/block/mmcblk3p9
/dev/block/mmcblk3p6 /cache ext4 rw,nosuid,nodev,nomblk_io_submit wait
/dev/block/mmcblk3p7 /device ext4 rw,nosuid,nodev wait
/dev/block/mmcblk3p1 /boot emmc defaults defaults
/dev/block/mmcblk3p2 /recovery emmc defaults defaults
/dev/block/mmcblk3p8 /misc emmc defaults defaults
But with out doing this change first i fallowed below procedure to build images for SD card booting i faced same issue.
remove out/target/product/sabresd_6dq/root directory and boot*.img
remove /out/target/product/sabresd_6dq/recovery directory and recovery*.img
remove /out/target/product/sabresd_6dq/system directory and system*.img
$ make BUILD_TARGET_DEVICE=sd
Thanks & Regards,
pushpa teja