I am porting Android Pie to Nitrogen6x(Boundary Devices) Board.
All images created and flashed to SD card.
But the device is not booting. The logs are given.
I think the error is on "fstab", filesystem mounting.
Can anybody help me to solve the same.......
Logs start here>>>>>>>>>>>>>>>>>
U-Boot 2018.07-35627-g23d0f45-dirty (Aug 21 2019 - 16:35:39 +0530)
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
Reset cause: WDOG
Board: nitrogen6x
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from SPI Flash...
SF: Detected sst25vf016b with page size 256 Bytes, erase size 4 KiB, total 2 MiB
OK
No match, assuming mode_str: 1920x1080M@30
In: serial
Out: serial
Err: serial
Net: Micrel ksz9021 at 6
FEC [PRIME], usb_ether
Hit any key to stop autoboot: 0
MMC: no card present
switch to partitions #0, OK
mmc1 is current device
Scanning mmc 1:1...
Found U-Boot script /boot.scr
4808 bytes read in 29 ms (161.1 KiB/s)
## Executing script at 10008000
** File not found uEnv.txt **
53553 bytes read in 79 ms (661.1 KiB/s)
only CEA modes allowed on HDMI port
btmac=00:19:b8:b3:3e:15
10037632 bytes read in 498 ms (19.2 MiB/s)
1956183 bytes read in 136 ms (13.7 MiB/s)
Kernel image @ 0x10800000 [ 0x000000 - 0x992980 ]
## Loading init Ramdisk from Legacy Image at 13800000 ...
Image Name: RAM Disk
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 1956119 Bytes = 1.9 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 13000000
Booting using the fdt blob at 0x13000000
reserving fdt memory region: addr=13000000 size=e000
Using Device Tree in place at 13000000, end 13010fff
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 4.9.88-g0bdac1b-dirty (sunilsharmap@lp-sunilsharmap) (gcc version 4.9.x 20150123 (prerelease) (GCC) ) #1 SMP PREEMPT Mon Aug 19 2
2:38:04 IST 2019
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
OF: fdt:Machine model: Boundary Devices i.MX6 Quad Nitrogen6x Board
cma: Reserved 448 MiB at 0x2a000000
Memory policy: Data cache writealloc
percpu: Embedded 15 pages/cpu @f6eb4000 s31116 r8192 d22132 u61440
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260368
Kernel command line: mxc_hdmi.only_cea=1 tsc2004.calibration=-67247,-764,272499173,324,69283,-8653010,65536 console=ttymxc1,115200 vmalloc=128M
consoleblank=0 rootwait androidboot.hardware=freescale androidboot.soc=i.MX6Q androidboot.bootdevice=2100000.aips-bus/219c000.usdhc androidboo
t.serialno=0019b8033e15 wlcore.mac=00:19:b8:83:3e:15 androidboot.wlan.mac=00:19:b8:83:3e:15 androidboot.btmacaddr=00:19:b8:b3:3e:15 cma=448M
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 555256K/1048576K available (13312K kernel code, 1205K rwdata, 4380K rodata, 1024K init, 590K bss, 34568K reserved, 458752K cma-reserved
, 139264K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xf8000000 - 0xff800000 ( 120 MB)
lowmem : 0xc0000000 - 0xf7800000 ( 888 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0xc0008000 - 0xc0e00000 (14304 kB)
.init : 0xc1400000 - 0xc1500000 (1024 kB)
.data : 0xc1500000 - 0xc162d600 (1206 kB)
.bss : 0xc162f000 - 0xc16c28bc ( 591 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
Build-time adjustment of leaf fanout to 32.
NR_IRQS:16 nr_irqs:16 16
L2C-310 errata 752271 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 16 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 16 ways, 1024 kB
L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76470001
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Security Framework initialized
SELinux: Initializing.
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
CPU: Testing write buffer coherency: ok
ftrace: allocating 38982 entries in 115 pages
CPU0: update cpu_capacity 1024
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10100000 - 0x10100058
CPU1: update cpu_capacity 1024
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU2: update cpu_capacity 1024
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU3: update cpu_capacity 1024
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
Brought up 4 CPUs
SMP: Total of 4 processors activated (24.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
CPU3: update max cpu_capacity 1024
devtmpfs: initialized
CPU2: update max cpu_capacity 1024
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 1024 (order: 4, 65536 bytes)
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor menu
CPU identified as i.MX6Q, silicon rev 1.2
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
imx-gpc 20dc000.gpc: no fsl,ldo-bypass found!
imx-gpc 20dc000.gpc: Registered imx-gpc
mxs-dma 110000.dma-apbh: initialized
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 28, base_baud = 5000000) is a IMX
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 77, base_baud = 5000000) is a IMX
console [ttymxc1] enabled
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 78, base_baud = 5000000) is a IMX
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
imx-i2c 21a0000.i2c: stop-delay=0, inter-byte-delay=0
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA, using PIO instead.
imx-i2c 21a4000.i2c: stop-delay=0, inter-byte-delay=0
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA, using PIO instead.
imx-i2c 21a8000.i2c: stop-delay=0, inter-byte-delay=0
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA, using PIO instead.
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
imx rpmsg driver is registered.
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.22
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
clocksource: Switched to clocksource mxc_timer1
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 1912K
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
Bus freq driver module loaded
audit: initializing netlink subsys (disabled)
audit: type=2000 audit(1.380:1): initialized
workingset: timestamp_bits=30 max_order=18 bucket_order=0
squashfs: version 4.0 (2009/01/31) Phillip Lougher
Registering sdcardfs 0.1
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
ntfs: driver 2.1.32 [Flags: R/W DEBUG].
fuse init (API version 7.26)
bounce: pool size: 64 pages
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
OF: PCI: host bridge /soc/pcie@0x01000000 ranges:
OF: PCI: No bus range found for /soc/pcie@0x01000000, using [bus 00-ff]
OF: PCI: IO 0x01f80000..0x01f8ffff -> 0x00000000
OF: PCI: MEM 0x01000000..0x01efffff -> 0x01000000
imx6q-pcie 1ffc000.pcie: phy link never came up
imx6q-pcie 1ffc000.pcie: Link never came up
imx6q-pcie 1ffc000.pcie: failed to initialize host
imx6q-pcie: probe of 1ffc000.pcie failed with error -110
ldb 2000000.aips-bus:ldb@020e0008: failed to find valid LVDS channel
ldb: probe of 2000000.aips-bus:ldb@020e0008 failed with error -22
20e0000.hdmi_video supply HDMI not found, using dummy regulator
mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
fbcvt: Refresh rate not CVT standard
fbcvt: 1920x1080@30: CVT Name - Not a CVT standard - 2.073 Mega Pixel Image
mxc_sdc_fb fb@2: registered mxc display driver hdmi
mxc_sdc_fb fb@2: 1920x1080 h_sync,r,l: 44,88,148 v_sync,l,u: 5,4,36 pixclock=74250000 Hz
imx-ipuv3 2800000.ipu: try ipu internal clk
imx-ipuv3 2800000.ipu: disp=0, pixel_clk=74250000 74250000 parent=74250000 div=1
find_field: [0] = 0x7ff, max=23
find_field: [1] = 0xfff, max=23
find_field: [2] = 0x17ff, max=23
find_field: [0] = 0x820, max=29
imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
mxc_sdc_fb fb@2: 1920x1080 h_sync,r,l: 44,88,148 v_sync,l,u: 5,4,36 pixclock=74250000 Hz
imx-ipuv3 2800000.ipu: try ipu internal clk
imx-ipuv3 2800000.ipu: disp=0, pixel_clk=74250000 74250000 parent=74250000 div=1
Console: switching to colour frame buffer device 240x67
add tfp410 i2c driver
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: loaded firmware 3.3
max7w-uart: version 1.0
driver magdecode registered
imx sema4 driver is registered.
[drm] Initialized
[drm] Initialized vivante 1.0.0 20120216 on minor 0
random: fast init done
brd: module loaded
loop: module loaded
zram: Added device: zram0
(stk) :sysfs entries created
(hci_tty): inside hci_tty_init
(hci_tty): allocated 242, 0
[max77823_init] start
ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024
ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480
ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000
ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000
ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled
ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
scsi host0: ahci-imx
ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 85
m25p80 spi0.0: sst25vf016b (2048 Kbytes)
3 ofpart partitions found on MTD device spi0.0
Creating 3 MTD partitions on "spi0.0":
0x000000000000-0x0000000c0000 : "U-Boot"
0x0000000c0000-0x0000000c2000 : "env"
0x0000000c2000-0x000000200000 : "splash"
spi_imx 2008000.ecspi: probed
libphy: Fixed MDIO Bus: probed
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
CAN device driver interface
2090000.flexcan supply xceiver not found, using dummy regulator
flexcan 2090000.flexcan: device registered (reg_base=f82ec000, irq=36)
2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
libphy: fec_enet_mii_bus: probed
mdio_bus 2188000.ethernet-1: /soc/aips-bus@02100000/ethernet@02188000/mdio/ethernet-phy has invalid PHY address
fec 2188000.ethernet eth0: registered PHC device 0
mxc_sdc_fb fb@2: 1920x1080 h_sync,r,l: 44,528,148 v_sync,l,u: 5,4,36 pixclock=148500000 Hz
PPP generic driver version 2.4.2
imx-ipuv3 2800000.ipu: try ipu internal clk
PPP BSD Compression module registered
PPP Deflate Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver
usbcore: registered new interface driver pegasus
usbcore: registered new interface driver rtl8150
usbcore: registered new interface driver r8152
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver cdc_eem
usbcore: registered new interface driver smsc95xx
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver cdc_acm
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usbserial
usbcore: registered new interface driver usbserial_generic
usbserial: USB Serial support registered for generic
usbcore: registered new interface driver cp210x
usbserial: USB Serial support registered for cp210x
usbcore: registered new interface driver ftdi_sio
usbserial: USB Serial support registered for FTDI USB Serial Device
usbcore: registered new interface driver keyspan
usbserial: USB Serial support registered for Keyspan - (without firmware)
usbserial: USB Serial support registered for Keyspan 1 port adapter
usbserial: USB Serial support registered for Keyspan 2 port adapter
usbserial: USB Serial support registered for Keyspan 4 port adapter
usbcore: registered new interface driver option
usbserial: USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver pl2303
usbserial: USB Serial support registered for pl2303
usbcore: registered new interface driver qcserial
usbserial: USB Serial support registered for Qualcomm USB modem
usbcore: registered new interface driver usb_ehset_test
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
setup_reset_gpios:-2, flags 0
setup_reset_gpios:204, flags 1
imx-ipuv3 2800000.ipu: disp=0, pixel_clk=148500000 148500000 parent=148500000 div=1
setup_reset_gpios:-2, flags 1
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
usbcore: registered new interface driver xpad
usbcore: registered new interface driver usb_acecad
usbcore: registered new interface driver aiptek
usbcore: registered new interface driver gtco
usbcore: registered new interface driver hanwang
usbcore: registered new interface driver kbtab
egalax_ts 2-0004: Failed to switch to I2C interface
ft5x06-ts 2-0038: reset fffffffe
ft5x06-ts 2-0038: Could not detect touch screen -19.
irq: type mismatch, failed to map hwirq-9 for /soc/aips-bus@02000000/gpio@0209c000!
Goodix-TS 2-0014: i2c test failed attempt 1: -6
Goodix-TS 2-0014: i2c test failed attempt 2: -6
Goodix-TS 2-0014: I2C communication failure: -6
irq: type mismatch, failed to map hwirq-9 for /soc/aips-bus@02000000/gpio@0209c000!
ata1: SATA link down (SStatus 0 SControl 300)
ahci-imx 2200000.sata: no device found, disabling link.
ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug
Goodix-TS 2-005d: i2c test failed attempt 1: -6
usb 1-1: new high-speed USB device number 2 using ci_hdrc
Goodix-TS 2-005d: i2c test failed attempt 2: -6
Goodix-TS 2-005d: I2C communication failure: -6
ili210x_i2c 2-0041: No platform data!
ili210x_i2c 2-0041: i2c transfer failed
ili210x_i2c 2-0041: Failed to get firmware version, err: -5
ili210x_i2c: probe of 2-0041 failed with error -5
tsc2004 2-0048: no vio regulator found
tsc2004 2-0048: tsc2004_cmd: failed, command: 1 i2c error: -6
tsc2004 2-0048: Device not present: -6
rtc-isl1208 0-006f: rtc core: registered rtc-isl1208 as rtc0
check_alarm_past: alarm in the past
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc1
i2c /dev entries driver
mxc_v4l2_output v4l2_out: V4L2 device registered as video16
mxc_v4l2_output v4l2_out: V4L2 device registered as video17
hub 1-1:1.0: USB hub found
hub 1-1:1.0: 3 ports detected
mxc_sdc_fb fb@2: 640x480 h_sync,r,l: 96,16,48 v_sync,l,u: 2,10,33 pixclock=25175000 Hz
imx-ipuv3 2800000.ipu: try ipu internal clk
imx-ipuv3 2800000.ipu: disp=0, pixel_clk=25175000 25142857 parent=264000000 div=10
mxc_sdc_fb fb@2: 1920x1080 h_sync,r,l: 44,528,148 v_sync,l,u: 5,4,36 pixclock=148500000 Hz
imx-ipuv3 2800000.ipu: try ipu internal clk
imx-ipuv3 2800000.ipu: disp=0, pixel_clk=148500000 148500000 parent=148500000 div=1
ov5640_read_reg:reg=300a ret=-6
camera ov5640 is not found, (fffffffa)
update_device_addr: ov5642 ret=-6
ov5642_read_reg:write reg error:reg=300a
camera ov5642 is not found(-1) 5a
update_device_addr: ov5640_mipi ret=-6
ov5640_read_reg(mipi):reg=300a ret=-6
camera ov5640_mipi is not found
tc358743_mipi 1-000f: no sensor pwdn pin available
1-000f supply DGPO not found, using dummy regulator
tc358743_read_reg:reg=0 ret=-6
tc358743_probe:cannot find camera
tc358743_probe: failed, error=-19
adv7180 2-0020: adv7180_get_gpios: pwn-gpios flags(1 -> 0)
adv7180 2-0020: adv7180_get_gpios: rst-gpios flags(1 -> 0)
adv7180_gpio_state: active=0, rst-gpios(78)=0x1
adv7180_probe: cea861=0
adv7180_gpio_state: active=0, pwn-gpios(77)=0x1
adv7180 2-0020: get mclk failed
adv7180 2-0020: adv7180_read:read reg error: reg=11 ret=-6
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
fake_poweroff_probe: found watchdog 20bc000.wdog
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.35.0-ioctl (2016-06-23) initialised: dm-devel@redhat.com
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol LL registered
usbcore: registered new interface driver btusb
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
(stc): chnl_id list empty :4
(stk) : st_kim_start
(stk) :ldisc_install = 1
mmc2: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
sdhci-esdhc-imx 2198000.usdhc: could not get ultra high speed state, work on normal mode
sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO
mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
sdhci-esdhc-imx 219c000.usdhc: could not get ultra high speed state, work on normal mode
sdhci-esdhc-imx 219c000.usdhc: Got CD GPIO
mmc1: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
mxc_vpu 2040000.vpu_fsl: VPU initialized
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
Galcore version 6.2.2.96445
mmc1: host does not support reading read-only switch, assuming write-enable
mmc1: new high speed SDHC card at address aaaa
mmcblk1: mmc1:aaaa SS16G 14.8 GiB
mmcblk1: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10
caam 2100000.caam: ERA source: CAAMVID.
caam 2100000.caam: AXI pipeline throttling enabled.
caam 2100000.caam: Entropy delay = 3200
caam 2100000.caam: Instantiated RNG4 SH0
caam 2100000.caam: Instantiated RNG4 SH1
caam 2100000.caam: device ID = 0x0a16010000000000 (Era 4)
caam 2100000.caam: job rings = 2, qi = 0
caam algorithms registered in /proc/crypto
caam_jr 2101000.jr0: registering rng-caam
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
ion_parse_dt_heap_common: id 0 type 4 name cma align 1000
ion_parse_dt_heap_common: id 1 type 4 name sys-contig align 1000
ion_parse_dt_heap_common: id 2 type 4 name system align 1000
ashmem: initialized
max77823_fuelgauge_init:
max77823_charger_init :
usbcore: registered new interface driver snd-usb-audio
sgtl5000 0-000a: sgtl5000 revision 0x11
sgtl5000 0-000a: Using internal LDO instead of VDDD: check ER1
(stk) :ldisc installation timeout
(stk) :ldisc_install = 0
fsl-ssi-dai 2028000.ssi: No cache defaults, reading back from HW
fsl-ssi-dai 202c000.ssi: No cache defaults, reading back from HW
imx-sgtl5000 sound: sgtl5000 <-> 2028000.ssi mapping ok
imx-sgtl5000 sound: ASoC: Cannot get gpio at index 0: -2
imx-audio-hdmi sound-hdmi: hdmi-hifi.0 <-> soc:hdmi_audio@00120000 mapping ok
NET: Registered protocol family 26
u32 classifier
Actions configured
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
ctnetlink v0.93: registering with nfnetlink.
xt_time: kernel timezone is -0000
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: arp_tables: (C) 2002 David S. Miller
Initializing XFRM netlink socket
NET: Registered protocol family 10
mip6: Mobile IPv6
ip6_tables: (C) 2000-2006 Netfilter Core Team
sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20161123 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
cpu cpu0: Registered imx6q-cpufreq
registered taskstats version 1
imx_thermal 2000000.aips-bus:tempmon: Automotive CPU temperature grade - max:125C critical:120C passive:115C
input: gpio-keys as /devices/soc0/gpio-keys/input/input2
rtc-isl1208 0-006f: hctosys: unable to read the hardware clock
usb_otg_vbus: disabling
reg_wlan_vmmc: disabling
ALSA device list:
#0: sgtl5000-audio
#1: imx-hdmi-soc
Freeing unused kernel memory: 1024K
init: init first stage started!
init: Using Android DT directory /proc/device-tree/firmware/android/
init: First stage mount skipped (missing/incompatible fstab in device tree)
init: Skipped setting INIT_AVB_VERSION (not in recovery mode)
init: Loading SELinux policy
audit: type=1403 audit(5.700:2): policy loaded auid=4294967295 ses=4294967295
selinux: SELinux: Loaded policy from /sepolicy
audit: type=1404 audit(5.720:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295
selinux: SELinux: Loaded file_contexts
init: init second stage started!
init: Using Android DT directory /proc/device-tree/firmware/android/
selinux: SELinux: Loaded file_contexts
init: Running restorecon...
selinux: SELinux: Could not stat /dev/block: No such file or directory.
init: waitid failed: No child processes
init: Couldn't load property file '/system/etc/prop.default': open() failed: No such file or directory: No such file or directory
init: Couldn't load property file '/prop.default': open() failed: No such file or directory: No such file or directory
init: Couldn't load property file '/product/build.prop': open() failed: No such file or directory: No such file or directory
init: Couldn't load property file '/odm/default.prop': open() failed: No such file or directory: No such file or directory
ueventd: ueventd started!
selinux: SELinux: Loaded file_contexts
ueventd: Parsing file /ueventd.rc...
ueventd: Parsing file /vendor/ueventd.rc...
ueventd: Unable to read config file '/vendor/ueventd.rc': open() failed: No such file or directory
ueventd: Parsing file /odm/ueventd.rc...
ueventd: Unable to read config file '/odm/ueventd.rc': open() failed: No such file or directory
ueventd: Parsing file /ueventd.freescale.rc...
ueventd: [libfs_mgr]fs_mgr_read_fstab_dt(): failed to read fstab from dt
ueventd: Coldboot took 0.202 seconds
audit: type=1400 audit(6.190:4): avc: denied { write } for pid=1 comm="init" name="alignment" dev="proc" ino=4026531977 scontext=u:r:init:s0
tcontext=u:object_r:proc:s0 tclass=file permissive=0
audit: type=1400 audit(6.220:5): avc: denied { write } for pid=1 comm="init" name="cursor_blink" dev="sysfs" ino=8446 scontext=u:r:init:s0 t
context=u:object_r:sysfs:s0 tclass=file permissive=0
audit: type=1400 audit(6.240:6): avc: denied { write } for pid=1 comm="init" name="bind" dev="sysfs" ino=11795 scontext=u:r:init:s0 tcontext
=u:object_r:sysfs:s0 tclass=file permissive=0
watchdogd: watchdogd started (interval 10, margin 20)!
file system registered
using random self ethernet address
using random host ethernet address
zram0: detected capacity change from 0 to 314572800
mkswap: executing /system/bin/mkswap failed: No such file or directory
mkswap: mkswap terminated by exit(255)
Unable to find swap-space signature
(stk) : timed out waiting for ldisc to be un-installedaudit: type=1400 audit(6.360:7): avc: denied { write } for pid=1 comm="init" name="rea
d_ahead_kb" dev="sysfs" ino=17409 scontext=u:r:init:s0 tcontext=u:object_r:sysfs:s0 tclass=file permissive=0
audit: type=1400 audit(6.380:8): avc: denied { write } for pid=1 comm="init" name="gpu3DMinClock" dev="sysfs" ino=17126 scontext=u:r:init:s0
tcontext=u:object_r:sysfs:s0 tclass=file permissive=0
(stk) :ldisc_install = 1(stk) :ldisc installation timeout
(stk) :ldisc_install = 0(stk) : timed out waiting for ldisc to be un-installed
(stk) :ldisc_install = 1(stk) :ldisc installation timeout
(stk) :ldisc_install = 0(stk) : timed out waiting for ldisc to be un-installed
(stk) :ldisc_install = 1(stk) :ldisc installation timeout
(stk) :ldisc_install = 0(stk) : timed out waiting for ldisc to be un-installed
(stk) :ldisc_install = 1(stk) :ldisc installation timeout
(stk) :ldisc_install = 0(stk) : timed out waiting for ldisc to be un-installed
(stk) :ldisc_install = 1(stk) :ldisc installation timeout
(stk) :ldisc_install = 0(stk) : timed out waiting for ldisc to be un-installed
Bluetooth: st_register failed -22
Hi Sunil,
The Nitrogen6X board is from our partner Boundary Devices, and they already provide Android 8.0.0, 7.1.1 and 6.0.1 images:
https://boundarydevices.com/wiki/nitrogen6x/
In case of having troubles with this board and its software, it is recommended contacting the support of Boundary Devices:
https://boundarydevices.com/support/
Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------