I am trying to boot Android Lollipop 5.0.2 in Freescale MCIMX6Q-SDP board. I have followed the Android User's guide document downloaded from freescale site for bsp download,build operations.
I was able to compile the source code successfully and the generated images are flashed using dd command. But during booting the system is hanging with "binder: 148:148 transaction failed 29189, size 0-0" error . The log is below.
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
mag3110 2-000e: check mag3110 chip ID
input: FreescaleMagnetometer as /devices/virtual/input/input3
input: eCompass as /devices/virtual/input/input4
mag3110 2-000e: mag3110 is probed
input: FreescaleAccelerometer as /devices/virtual/input/input5
mma8x5x device driver probe successfully
imx2-wdt 20c0000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.24.0-ioctl (2013-01-15) initialised: dm-devel@redhat.com
Bluetooth: Virtual HCI driver ver 1.3
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCIATH3K protocol initialized
usbcore: registered new interface driver btusb
cpuidle: using governor ladder
cpuidle: using governor menu
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc1: no vqmmc regulator found
mmc1: no vmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
mmc2: no vqmmc regulator found
mmc2: no vmmc regulator found
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmc3: no vqmmc regulator found
mmc3: no vmmc regulator found
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
mmc2: new high speed SDHC card at address aaaa
Galcore version 5.0.11.25762
mmcblk2: mmc2:aaaa SS04G 3.69 GiB
mmcblk2: p1 p2 p3 < p5 p6 p7 p8 p9 > p4
mmcblk2: p4 size 5567104 extends beyond EOD, truncated
mmc3: BKOPS_EN bit is not set
mmc3: new high speed DDR MMC card at address 0001
mmcblk3: mmc3:0001 SEM08G 7.39 GiB
mmcblk3boot0: mmc3:0001 SEM08G partition 1 2.00 MiB
mmcblk3boot1: mmc3:0001 SEM08G partition 2 2.00 MiB
mmcblk3rpmb: mmc3:0001 SEM08G partition 3 128 KiB
mmcblk3: p1 p2
mmcblk3boot1: unknown partition table
mmcblk3boot0: unknown partition table
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_asrc 2034000.asrc: mxc_asrc registered
mxc_vpu 2040000.vpu: VPU initialized
hidraw: raw HID events driver (C) Jiri Kosina
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
ashmem: initialized
logger: created 256K log 'log_main'
logger: created 256K log 'log_events'
logger: created 256K log 'log_radio'
logger: created 256K log 'log_system'
usbcore: registered new interface driver snd-usb-audio
wm8962 0-001a: customer id 0 revision D
fsl-hdmi-dai hdmi_audio.17: failed to probe. Load HDMI-video first.
fsl-hdmi-dai: probe of hdmi_audio.17 failed with error -12
input: WM8962 Beep Generator as /devices/soc0/soc.1/2100000.aips-bus/21a0000.i2c/i2c-0/0-001a/input/input6
imx-wm8962 sound.28: wm8962 <-> 202c000.ssi mapping ok
imx-audio-hdmi sound-hdmi.29: initialize HDMI-audio failed. load HDMI-video first!
NET: Registered protocol family 26
u32 classifier
Actions configured
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (15956 buckets, 63824 max)
ctnetlink v0.93: registering with nfnetlink.
NF_TPROXY: Transparent proxy support initialized, version 4.1.0
NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
xt_time: kernel timezone is -0000
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: (C) 2002 David S. Miller
TCP: cubic registered
Initializing XFRM netlink socket
NET: Registered protocol family 10
mip6: Mobile IPv6
ip6_tables: (C) 2000-2006 Netfilter Core Team
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
VGEN1: disabling
SWBST: disabling
SW4: disabling
wm8962-supply: disabling
usb_otg_vbus: disabling
regulator-dummy: disabling
imx mcc test is registered.
UBI error: ubi_init: UBI error: cannot initialize UBI, error -19
file system registered
android_usb gadget: Mass Storage Function, version: 2009/09/11
android_usb gadget: Number of LUNs=1
lun0: LUN: removable file: (no medium)
android_usb gadget: android_usb ready
input: gpio-keys.27 as /devices/soc0/gpio-keys.27/input/input7
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:05:00 UTC (300)
ALSA device list:
#0: wm8962-audio
Freeing unused kernel memory: 340K (80e7b000 - 80ed0000)
type=1403 audit(300.720:2): policy loaded auid=4294967295 ses=4294967295
type=1404 audit(300.730:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295
init: /dev/hw_random not found
Console: switching to colour dummy device 80x30
init: /dev/hw_random not found
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
fs_mgr: Could not open block device /dev/block/mmcblk3p5 (No such file or directory).
fs_mgr: Could not set up verified partition, skipping!
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
fs_mgr: __mount(source=/dev/block/mmcblk3p4,target=/data,type=ext4)=-1
fs_mgr: fs_mgr_mount_all(): possibly an encryptable blkdev /dev/block/mmcblk3p4 for mount /data type ext4 )
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
fs_mgr: __mount(source=/dev/block/mmcblk3p6,target=/cache,type=ext4)=-1
fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk3p6 at /cache options: nomblk_io_submit error: No such file or directory
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
fs_mgr: __mount(source=/dev/block/mmcblk3p7,target=/device,type=ext4)=-1
fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk3p7 at /device options: (null) error: No such file or directory
init: fs_mgr_mount_all returned an error
init: fs_mgr_mount_all returned unexpected error 255
SELinux: Could not set context for /cache: Read-only file system
rfkill: BT RF going to : off
init: cannot find '/system/bin/logd', disabling 'logd'
init: cannot find '/system/bin/lmkd', disabling 'lmkd'
binder: 148:148 transaction failed 29189, size 0-0
init: cannot find '/system/bin/servicemanager', disabling 'servicemanager'
init: cannot find '/system/bin/vold', disabling 'vold'
init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger'
init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead
init: property 'ro.serialno' doesn't exist while expanding '$ro.serialno'
init: cannot expand '$ro.serialno' while writing to '/sys/class/android_usb/android0/iSerial'
init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead
init: property 'ro.product.manufacturer' doesn't exist while expanding '$ro.product.manufacturer'
init: cannot expand '$ro.product.manufacturer' while writing to '/sys/class/android_usb/android0/iManufacturer'
init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
init: property 'ro.product.model' doesn't exist while expanding '$ro.product.model'
init: cannot expand '$ro.product.model' while writing to '/sys/class/android_usb/android0/iProduct'
android_usb: already disabled
mtp_bind_config
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
binder: 148:148 transaction failed 29189, size 0-0
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
binder: 148:148 transaction failed 29189, size 0-0
I also tried with booting the prebuilt images "android_L5.0.0_1.0.0-ga_images_6qsabresd.tar.gz". This was booting even though I am getting some similiar prints shown below
Freeing unused kernel memory: 340K (80e7b000 - 80ed0000)
init: /dev/hw_random not found
Console: switching to colour dummy device 80x30
init: /dev/hw_random not found
EXT4-fs (mmcblk2p5): mounted filesystem with ordered data mode. Opts: barrier=1
fs_mgr: __mount(source=/dev/block/mmcblk2p5,target=/system,type=ext4)=0
EXT4-fs (mmcblk2p4): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk2p4): recovery complete
EXT4-fs (mmcblk2p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
fs_mgr: __mount(source=/dev/block/mmcblk2p4,target=/data,type=ext4)=0
EXT4-fs (mmcblk2p6): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk2p6): recovery complete
EXT4-fs (mmcblk2p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
fs_mgr: __mount(source=/dev/block/mmcblk2p6,target=/cache,type=ext4)=0
EXT4-fs (mmcblk2p7): mounted filesystem with ordered data mode. Opts: (null)
fs_mgr: __mount(source=/dev/block/mmcblk2p7,target=/device,type=ext4)=0
rfkill: BT RF going to : off
binder: 157:157 transaction failed 29189, size 0-0
init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead
init: property 'ro.serialno' doesn't exist while expanding '$ro.serialno'
init: cannot expand '$ro.serialno' while writing to '/sys/class/android_usb/android0/iSerial'
init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead
init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
init: cannot find '/system/bin/debuggerd64', disabling 'debuggerd64'
init: cannot find '/system/bin/install-recovery.sh', disabling 'flash_recovery'
android_usb: already disabled
mtp_bind_config
root@sabresd_6dq:/ # healthd: BatteryTemperaturePath not found
healthd: BatteryTechnologyPath not found
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
warning: `main' uses 32-bit capabilities (legacy support in use)
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
period 165695543 ,timeout is 165704133, wake up is :0
period 165695543 ,timeout is 165704133, wake up is :0
request_suspend_state: wakeup (3->0) at 15323264001 (1970-01-01 00:00:11.618185001 UTC)
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
lowmemorykiller: lowmem_shrink: convert oom_adj to oom_score_adj:
lowmemorykiller: oom_adj 0 => oom_score_adj 0
lowmemorykiller: oom_adj 1 => oom_score_adj 58
lowmemorykiller: oom_adj 2 => oom_score_adj 117
lowmemorykiller: oom_adj 3 => oom_score_adj 176
lowmemorykiller: oom_adj 9 => oom_score_adj 529
lowmemorykiller: oom_adj 15 => oom_score_adj 1000
acc_open
acc_release
fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
binder: undelivered transaction 3155
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
period 66 ,timeout is 0, wake up is :0
mma enable setting active
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
rfkill: BT RF going to : off
rfkill: BT RF going to : on
mxc_bt_rfkill_reset
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
I have added the "androidboot.selinux=disabled androidboot.dm_verity=disabled" as boot argument to make the prebuilt images to boot. But setting the same boot argument in the built image gives no positive result. Any help would be appreciated....
Hi,
The default images that you build works for the eMMC but to boot the image from the SD card, you need to follow the below instructions:
3.4.3 Building Android image for the SD card on the SABRE-SD
Board
The default configuration in the source code package takes internal eMMC as the boot storage. It can be changed to make the
SD card in SD Slot 3 as the boot storage as follows:
remove out/target/product/sabresd_6dq/root directory and boot*.img
remove /out/target/product/sabresd_6dq/recovery directory and recovery*.img
remove /out/target/product/sabresd_6dq/system directory and system*.img
$ make BUILD_TARGET_DEVICE=sd
Follow Section 3.4 to build the images.
For more information please refer to the Android_User_Guide.pdf from the documentation section.
Thanks and Regards,
-Devaraj
Android 5.0.2 is still in alpha testing and not released to the public yet.
Please contact the FAE that shared the BSP with you to receive support.