Hi EveryOne,
This is my follow up question to below thread
Slow H264 1080P@60fps Decoding on Android Lollipop 5.0.2 SabreSD
On the path of debugging the root cause of above issue, I tried various approach to Decode 1080P at 60 FPS.
1. I tried wrapping H264 data into a MP4 container(without transcoding). The playback of MP4 with various stock player seems slow(less than 60fps , around 42fps).
2. I tried using native codec samples from Android NDK. Still no progress.
3 Later I compiles the mxc-vpu-test code from the Android Source tree. With this and using the correct parameters, I was Capable of playing the video at 60 FPS.
So My doubts are
- Is the decoder capable of playing 1080p@60fps video, with correct Frame rate ?
- If so, then why MediaCodec ( using ACodec code internally ) is not capable of playing 1080p@60fps video.
- I am not sure if OMXCodec is used in this process, Where can I get OMXCodec sample code to decode my video.
Thanks
Gurtaj
Hi Gurtaj
omx player (as part of Freescale Enhanced Codecs) is provided in
Extended multimedia package, obtained separately using procedure described in
sect.6 Freescale Extended Feature Packages attached Release Notes.
Codecs performance (in fps) is described in attached i.MX_Android_Extended_
Codec_Release_Notes.pdf sect.5 Codec Specification.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thanks for the documents.
I want to use mediacodec for decoding 1080p@60 fps video. Seem like Freescale doesn't support it but still I am capable of playing this using mxc-vpu-test.
Can Someone explain me the difference between the MediaCodec and MXC-VP-TEST decoding techniques and why one is capable of decoding while other is not.
Regards & Thanks
Gurtaj
Igor,
No, I will disagree on that. As We can see from logcat logs , MediaCodec ( via ACodec ) selecting the hardware decoder OMX.Freescale.std.video_decoder.avc.v3.hw-based.
Can you point me to some test code which uses AwesomePlayer (OMXCodec ) for decoding and rendering. I want to verify other implementation and eliminate if there is any issue with using MediaCodec ( via ACodec ).
Regards,
Gurtaj
Gurtaj
omx player (as part of Freescale Enhanced Codecs) is provided in
Extended multimedia package, obtained separately using procedure described in
sect.6 Freescale Extended Feature Packages attached Release Notes.
~igor
Igor,
Sorry Sir, I am not getting any technical detail here.
I am not sure what has changed from Android Jeallybean-4.2.2_1.0.0-ga to Android Lollipop-5.0.2
that has suppress the capability of decoder (Using MediaCodec Interface ) to decode 1080p@60fps.
Can Someone please justify this difference ???
Regards,
Gurtaj