[Android 4.4.2] Preview and video recording issue on USB camera

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Android 4.4.2] Preview and video recording issue on USB camera

2,777件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP

I test USB camera (logitech webcam) in imx6 sabresd demo board (Android 4.4.2).

I used usb-hub to connect to OTG port. 

Because I need to connect usb camera ,usb mouse and keyboard. 

When I open camera apk and preview it, the picture is not correctly.

Please refer the attachment file.

VID_20160908_090232.3gpp is recording video.

pass.jpg is correct picture.

error.jpg is not correct picture.

Do you have any advice?

Clayder

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,557件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Are you having this problem only when you use the USB Hub?, or is it independent of it?

0 件の賞賛
返信

2,557件の閲覧回数
charleshuang
Senior Contributor II

Hi SerigioSolis

Yes, this problem only when I  use the USB HUB.  Because our application need to connect usb camera , usb mouse and usb keyboard in platform.

0 件の賞賛
返信