Android 11.0.0_2.2.0 on IMX8MP - 2 GB RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android 11.0.0_2.2.0 on IMX8MP - 2 GB RAM

529 Views
oferausterlitz
Senior Contributor II

Hi , 

We have two different boards 4GB RAM and 2 GB RAM

* 4 GB RAM android release perfectly works 

* 2 GB RAM android generates random crashes either in android service or kernel or sometimes.

Older release Android 11.0.0 1.2.0 works fine with 2GB without any problems. 

Majorly android services include which generates crash

 - Audio

- Graphics 

- Camera 

which requires more heap memory are the major when it generates segfaults. 

Attached is the log for 2GB memory device we are trying to get it stable. 

My question is Android 11.0.0. 2.2.0 validated on 2 GB EVK?

If validated then what could areas we can look to fix this? 

Is LOW_MEMORY:=true flag required for this ? If so we tried this but generates same crash. 

 

Thanks

Ofer

 

0 Kudos
Reply
1 Reply

479 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

BSP is tested on 6GB EVK.Can you try android11_2.6.0?

 

0 Kudos
Reply