Android 调用v4l2 JNI 显示卡顿

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android 调用v4l2 JNI 显示卡顿

1,659 Views
15203565340
Contributor II

我现在用V4L2编译了一个JNI库给我们的android工程师来调用来获取和显示摄像头数据,现在可以获取到画面,但画面卡到惨不忍睹,通过log看到1秒只能输出两、三帧,而时间主要消耗在yuyv422toABGRY()这个转换。而且CPU占用率高达50%左右。问了别人,说这种图像处理应该让GPU来处理。我想问应该怎么调用GPU来处理这个计算,还是说我的处理方法不对,有更好的方法呢。求大神们指教!!!

pastedImage_1.pngpastedImage_2.png

Labels (2)
Tags (1)
0 Kudos
3 Replies

1,504 Views
15203565340
Contributor II

现在画面确实卡顿十分严重,yuyv422toABGRY()这个编码过程太费时间和资源了。这个问题有什么好方法解决呢!!!求教。

0 Kudos

1,504 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello ydf123,

    I don't know which processor you are using. see below, please!

--i.MX6Q/D/DL/S

IPU & GPU are both supported by these 4 processors.

--i.mx7d/s

there are no IPU and GPU in these 2 processors.

--About android

Android requires that images must be handled by GPU.

--------------------------Chinese---------------

android对图像的处理,必须要通过GPU来处理的,所以您说的没有用到GPU的情况是不存在的。不清楚您在使用哪款处理器。如果是I.MX7D/S,那么它们内部是没有GPU和IPU的,而且,android for i.MX7d也不支持camera。

Have a nice day!

NXP TIC weidong sun

0 Kudos

1,504 Views
15203565340
Contributor II

你好,

   首先谢谢你的回复,我用的是imx6q,不知道imx6q内部有没有GPU和IPU呢。还有我有点不明白你的意思,你是说android在调用C编译的jNI时就已经在用GPU在处理了么。

0 Kudos