Altium Files for i.MX 8M Mini EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Altium Files for i.MX 8M Mini EVK

9,138件の閲覧回数
arun_panangala
Contributor II

Hello,

Is it possible for me get the Altium Design files for 8MMINILPD4-EVK SoM Board. I am unable to convert the Allegro files to Altium from the Data pack provided in the .zip file.

Kind Regards,

Arun

51 返答(返信)

3,615件の閲覧回数
rausov
Contributor I

I've the same problem too.

0 件の賞賛

3,091件の閲覧回数
b36401
NXP Employee
NXP Employee

Sorry, I did not find your email address in out database.
Please let me it know.

0 件の賞賛

3,057件の閲覧回数
afougerat
Contributor I

Dear Victor,

   Can I have also the  iMX8MMini Evk project  under Altium Design format ?  It will be nice for the futur to have this file format available for all new evk design.

Best regards

Arnaud

0 件の賞賛

3,050件の閲覧回数
b36401
NXP Employee
NXP Employee

Sorry, I did not find your email address in out database.
Please let me it know.

0 件の賞賛

3,025件の閲覧回数
b36401
NXP Employee
NXP Employee

OK. I sent the files.

0 件の賞賛

2,684件の閲覧回数
jacekskrzypiec
Contributor II

Hello,

     I would like to ask you to send me the Altium Design files for 8MMINILPD4-EVK SoM Board.

Thanks

0 件の賞賛

2,673件の閲覧回数
Yuri
NXP Employee
NXP Employee

@jacekskrzypiec 
Hello,

  please create separate thread / request.

Regards,
Yuri.

0 件の賞賛

3,017件の閲覧回数
torstenminas
Contributor I

Dear Victor,

can you also send us these files, please?

Best Regards

TM

2,962件の閲覧回数
b36401
NXP Employee
NXP Employee

I just replied your email and sent the files.

0 件の賞賛

2,940件の閲覧回数
torstenminas
Contributor I

Thank you!

But the files you have send are the cadence files. Can you please send me the files for Altium Designer?

Best regards

Torsten

0 件の賞賛

2,940件の閲覧回数
b36401
NXP Employee
NXP Employee

Hello Torsten,

Sorry, I did not find your email address in out database.
Please create a separate thread.

0 件の賞賛

2,942件の閲覧回数
sy_lau
Contributor I

Dear Victor,

Can we also have a copy of Altium design files for LPDDR and DDR EVKs, will be much helpful for us.

Thanks a lot.

Best Regards,

SY

2,940件の閲覧回数
b36401
NXP Employee
NXP Employee

Hello Seng-Yong,

I sent you the files to your e-mail address.

0 件の賞賛

2,940件の閲覧回数
kenny_wang1
Contributor I

Dear Victor,

      Please help send me  the Altium design files of  8MMINILPD4-CPU (SOM board) and 8MMINI-BB (base board).

        

Best Regards,

Kenny

0 件の賞賛

2,940件の閲覧回数
tom_perman
Contributor III

Can I be sent these files also? We would find these useful as we also use Altium for PCB Design

0 件の賞賛

2,940件の閲覧回数
b36401
NXP Employee
NXP Employee

Tom,

I sent you the file to your ...@garrison.com email. I hope it is right email.

2,945件の閲覧回数
ea_arun
Contributor I

Hi Victor,

Can yu please help me too with the Altium files of 8MMINI CAD files...If possible immediately...

Thanks and Regards,

Arun

0 件の賞賛

2,945件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please create separate request / thread. 

Support | NXP 

Regards,

Yuri.

0 件の賞賛

2,945件の閲覧回数
tom_perman
Contributor III

Thank you. I have received OK!

2,945件の閲覧回数
arun_panangala
Contributor II

Thanks ! b36401‌ much appreciated.

2,947件の閲覧回数
markushager
Contributor II

Dear Victor,

can you send me also Altium Files for i.MX 8M Mini EVK and i.MX 8M Nano EVK with DDR4 Memory?

thank you Markus

0 件の賞賛