Altium Files for IMX8M Nano DDR4 Evalboard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Altium Files for IMX8M Nano DDR4 Evalboard

3,371件の閲覧回数
markushager
Contributor II

Dear Victor, can you please send Altium Files for 8MNANOD4-EVK to th FTP account I sent you via email?

ラベル(1)
14 返答(返信)

2,612件の閲覧回数
Sal2020
Contributor II

0

タグ(2)

3,073件の閲覧回数
Ronak05
Contributor I

Hello NXP Techsupport Team,

 

I have been trying to import the design files for i.MX 8M Nano EVK  in Altium19 but while importing the files altium displays the error of files being old or unrecognized file type. 

 

Can you please email me the latest version altium files of this Eval kit ?

 

My email id is ronakk@acevin.com

0 件の賞賛

3,152件の閲覧回数
b36401
NXP Employee
NXP Employee

ftp> put 8MNDDR4.tar
local: 8MNDDR4.tar remote: 8MNDDR4.tar
200 PORT command successful
150 Opening BINARY mode data connection for 8MNDDR4.tar
226 Transfer complete
2600960 bytes sent in 4.09 secs (620.6434 kB/s)
ftp>

3,152件の閲覧回数
markushager
Contributor II

Thank you for the files!

0 件の賞賛

3,152件の閲覧回数
radias
Contributor II

Hi Markus,

Could you send me these files (Altium) in my email please?

radias@inatel.br

Thank you in advance.

0 件の賞賛

3,152件の閲覧回数
carlesre
Contributor II

Hi Ricardo,

could you send me these 8MNANOD4-EVK Altium files?

carles.recasens@wallbox.com

I would really appreciate that!

Thank you in advance

Carles

0 件の賞賛

3,156件の閲覧回数
radias
Contributor II

Hi Carles,

Files were sent to your email.

Let me know if they work fine.

Kind Regards.

Ricardo Antonio Dias

email: radias@inatel.br<mailto:radias@inatel.br> | skype: dias.a.ricardo

Tel: (35) 3471-9914 | ramal: 914

Antes de imprimir, pense em sua responsabilidade com o meio ambiente!

De: carlesre <admin@community.nxp.com>

Enviada em: sexta-feira, 5 de junho de 2020 11:54

Para: Ricardo Antonio Dias <radias@inatel.br>

Assunto: Re: - Re: Altium Files for IMX8M Nano DDR4 Evalboard

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Altium Files for IMX8M Nano DDR4 Evalboard

reply from Carles Recasens<https://community.nxp.com/people/carlesre?et=watches.email.thread> in i.MX Processors - View the full discussion<https://community.nxp.com/message/1322510?commentID=1322510&et=watches.email.thread#comment-1322510>

3,156件の閲覧回数
carlesre
Contributor II

Hi Ricardo,

I have received Altium files, they seem to be OK.

Thank you very much, I really appreciate your support!!

If I can help you with something, please let me know

Kind Regards,

Carles

0 件の賞賛

3,154件の閲覧回数
radias
Contributor II

Hi Carles,

Great to hear that.

Good to know that I have some on to help me if a I were in trouble.

Kind Regards,

Ricardo Antonio Dias

email: radias@inatel.br<mailto:radias@inatel.br> | skype: dias.a.ricardo

Tel: (35) 3471-9914 | ramal: 914

Antes de imprimir, pense em sua responsabilidade com o meio ambiente!

De: carlesre <admin@community.nxp.com>

Enviada em: segunda-feira, 8 de junho de 2020 04:10

Para: Ricardo Antonio Dias <radias@inatel.br>

Assunto: Re: - Re: Altium Files for IMX8M Nano DDR4 Evalboard

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Altium Files for IMX8M Nano DDR4 Evalboard

reply from Carles Recasens<https://community.nxp.com/people/carlesre?et=watches.email.thread> in i.MX Processors - View the full discussion<https://community.nxp.com/message/1323052?commentID=1323052&et=watches.email.thread#comment-1323052>

0 件の賞賛

3,154件の閲覧回数
radias
Contributor II

Hi Markus,

I'd like to ask you if you have de base board files to IMX8M Nano able to be imported into Altium also?

May you can send me this files?

Thank you in advance.

Best regards.

Ricardo Dias.

0 件の賞賛

3,154件の閲覧回数
radias
Contributor II

Hi Markus,

Thanks for sent files.

I already test them and they are all ok.

Best Regards,

Ricardo Dias.

0 件の賞賛

3,154件の閲覧回数
b36401
NXP Employee
NXP Employee

I just sent you the files.

0 件の賞賛

3,034件の閲覧回数
kbrakora
Contributor I

Hi Victor,

Could I get the Altium project files or the files in a format importable into Altium?  My e-mail address is kbrakora@btengin.com.

Best Regards,

Karl

0 件の賞賛

3,008件の閲覧回数
Yuri
NXP Employee
NXP Employee

@kbrakora 
Hello,

   it makes sense to create separate thread or request:

 

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu

 

Regards,
Yuri.

0 件の賞賛