Alternate functions of i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Alternate functions of i.MX6UL

478 Views
surendrajadhav
Contributor IV

Hello,

i.MX6UL has got Booting options where 24 LCD lines are used. At the start up, state of these pins are polled to select the booting device. However out of these, first two pins I have to use for I2C function where I need pull up on these lines. So if I put pull up on these lines, it will lead to disturb the booting mode. However datasheet and pin mapping excel suggest I can use I2C as alternate function also. Let me know how to handle this.

One more query was I am using PMIC PF3000 for powering the i.MX6UL. Can you review my PMIC and processor connection in the attached image?

Regards,

Surendra

Labels (1)
0 Kudos
1 Reply

338 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Please refer to https://community.nxp.com/thread/441350 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

 

0 Kudos