I used Yocto to build my image.
I use these for options:
MKUBIFS_ARGS = "-m 4096 -e 253952 -c 1932" UBINIZE_ARGS = "-p 256KiB -m 4096"
On booting Linux immediately after flashing my NAND, I see:
[ OK ] Started Flush Journal to Persistent Storage.
[ 9.208493] UBIFS error (ubi0:0 pid 149): ubifs_check_node: bad node length 32840
[ 9.225422] UBIFS error (ubi0:0 pid 149): ubifs_check_node: bad node at LEB 302:208896
[ 9.233369] magic 0x6101831
[ 9.237193] crc 0x4064dc01
[ 9.240959] node_type 2 (direntry node)
[ 9.245391] group_type 1 (in node group)
[ 9.249759] sqnum 59940
[ 9.253080] len 32840
[ 9.256447] key (5258, direntry, 0xbd23f8)
[ 9.261595] inum 6490
[ 9.264831] type 0
[ 9.267839] nlen 15
[ 9.270900] name .#gshadowYhgOMs
[ 9.335212] CPU: 0 PID: 149 Comm: systemd-sysuser Not tainted 5.4.24-2.1.0+gbabac008e5cf #1
[ 9.343593] Hardware name: Freescale i.MX6 Ultralite (Device Tree)
[ 9.349827] [<80111854>] (unwind_backtrace) from [<8010c3e8>] (show_stack+0x10/0x14)
If I then boot into U-Boot there are errors doing the mount, but if I re-flash, U-Boot can mount the UBIFS just fine and I can list directories.
It is also possible to boot my device from SD card. Here is what I see when booting from SD card:
root@imx6ull14x14evk:~# mtdinfo -u /dev/mtd0
mtd0
Name: gpmi-nand
Type: nand
Eraseblock size: 262144 bytes, 256.0 KiB
Amount of eraseblocks: 2048 (536870912 bytes, 512.0 MiB)
Minimum input/output unit size: 4096 bytes
Sub-page size: 4096 bytes
OOB size: 256 bytes
Character device major/minor: 90:0
Bad blocks are allowed: true
Device is writable: true
Default UBI VID header offset: 4096
Default UBI data offset: 8192
Default UBI LEB size: 253952 bytes, 248.0 KiB
Maximum UBI volumes count: 128
解決済! 解決策の投稿を見る。
This problem was due to incorrect flashing from U-Boot.
The Yocto build creates *.ubi and *.ubifs. The *.ubi file contains the volume information and the file systems. I was using nand write to write this image. U-Boot could mount the file system, and everything seems just fine in U-Boot, but you cannot boot a 2nd time and get the root file system to mount if you use the *.ubi file and write it with nand write.
I then found that if I use an SD card and boot to Linux, you could write the *.ubi file using ubiformat. Then remove the SD card, and boot over and over again using the NAND flash.
There does not seem to be a similar command to ubiformat in U-Boot. So I looked some more, and uboot has a function called ubi write, and it turns out that this command can write a UBI file system. So to write the UBI file system images using U-Boot I used the following commands (nandrootfs is the mtd partition name for my ubi partition):
FB: download -f core-image-minimal-test-imx6ull14x14evk.ubifs
FB[-t 25000]: ucmd ubi part nandrootfs
FB[-t 10000]: ucmd ubi create rootfs
FB[-t 10000]: ucmd ubi info l
FB[-t 10000]: ucmd ubi info
FB[-t 25000]: ucmd ubi write ${fastboot_buffer} rootfs ${fastboot_bytes}
FB[-t 10000]: ucmd ubifsmount ubi0:rootfs
FB: acmd reset
FB: Done
This problem was due to incorrect flashing from U-Boot.
The Yocto build creates *.ubi and *.ubifs. The *.ubi file contains the volume information and the file systems. I was using nand write to write this image. U-Boot could mount the file system, and everything seems just fine in U-Boot, but you cannot boot a 2nd time and get the root file system to mount if you use the *.ubi file and write it with nand write.
I then found that if I use an SD card and boot to Linux, you could write the *.ubi file using ubiformat. Then remove the SD card, and boot over and over again using the NAND flash.
There does not seem to be a similar command to ubiformat in U-Boot. So I looked some more, and uboot has a function called ubi write, and it turns out that this command can write a UBI file system. So to write the UBI file system images using U-Boot I used the following commands (nandrootfs is the mtd partition name for my ubi partition):
FB: download -f core-image-minimal-test-imx6ull14x14evk.ubifs
FB[-t 25000]: ucmd ubi part nandrootfs
FB[-t 10000]: ucmd ubi create rootfs
FB[-t 10000]: ucmd ubi info l
FB[-t 10000]: ucmd ubi info
FB[-t 25000]: ucmd ubi write ${fastboot_buffer} rootfs ${fastboot_bytes}
FB[-t 10000]: ucmd ubifsmount ubi0:rootfs
FB: acmd reset
FB: Done
It appears the problem is the ubi image. The following creates a correct image on the device (booted from SD card):
flash_erase /dev/mtd6 0 0
ubiformat /dev/mtd6
ubiattach /dev/ubi0 -m6
ubimkvol /dev/ubi0 -N root -s 150MiB
mkdir /run/root
mount -t ubifs ubi0:root /run/root/
cd /run/root
tar -xf /tmp/core-image-minimal-test-imx6ull14x14evk-20210415160553.rootfs.tar.gz
But if I use nand_write to write the image to /dev/mtd6, mount the root file system, and then try to use it, lots of ECC errors occur.
In mtd-utils-tests there is a program called runubitests.sh. This test passes, but requires deleting the volume created by U-Boot.
# ./runubitests.sh /dev/ubi0
Running mkvol_basic /dev/ubi0
Running mkvol_bad /dev/ubi0
Running mkvol_paral /dev/ubi0
Running rsvol /dev/ubi0
Running io_basic /dev/ubi0
Running io_read /dev/ubi0
Running io_update /dev/ubi0
Running io_paral /dev/ubi0
Running volrefcnt /dev/ubi0
SUCCESS
mkvol_bad test generated many log messages.
[ 1214.188146] ubi0 error: ubi_cdev_ioctl: bad volume creation request
[ 1214.215176] Volume creation request dump:
[ 1214.219221] vol_id -2
[ 1214.221849] alignment 1
[ 1214.262392] bytes 489111552
[ 1214.265651] vol_type 3
[ 1214.268192] name_len 22
[ 1214.270823] 1st 16 characters of name: mkvol_bad:test_m
[ 1214.305239] ubi0 error: ubi_cdev_ioctl: bad volume creation request
[ 1214.311536] Volume creation request dump:
[ 1214.344232] vol_id 128
[ 1214.346969] alignment 1
[ 1214.349511] bytes 489111552
[ 1214.376857] vol_type 3
[ 1214.379422] name_len 22
[ 1214.382055] 1st 16 characters of name: mkvol_bad:test_m
[ 1214.416760] ubi0 error: ubi_cdev_ioctl: bad volume creation request
[ 1214.441618] Volume creation request dump:
[ 1214.463337] vol_id 0
[ 1214.465902] alignment 0
[ 1214.468446] bytes 489111552
[ 1214.471681] vol_type 3
[ 1214.502296] name_len 22
[ 1214.504949] 1st 16 characters of name: mkvol_bad:test_m
[ 1214.510434] ubi0 error: ubi_cdev_ioctl: bad volume creation request
[ 1214.551208] Volume creation request dump:
[ 1214.562990] vol_id 0
[ 1214.565554] alignment -1
[ 1214.568184] bytes 489111552
[ 1214.571420] vol_type 3
[ 1214.594912] name_len 22
[ 1214.597565] 1st 16 characters of name: mkvol_bad:test_m
[ 1214.617108] ubi0 error: ubi_cdev_ioctl: bad volume creation request
[ 1214.634719] Volume creation request dump:
[ 1214.638765] vol_id 0
[ 1214.641307] alignment 253953
[ 1214.661658] bytes 489111552
[ 1214.672298] vol_type 3
[ 1214.674863] name_len 22
[ 1214.677494] 1st 16 characters of name: mkvol_bad:test_m
[ 1214.701828] ubi0 error: ubi_cdev_ioctl: bad volume creation request
[ 1214.720791] Volume creation request dump:
[ 1214.731061] vol_id 0
[ 1214.760617] alignment 4097
[ 1214.768935] bytes 489111552
[ 1214.779536] vol_type 3
[ 1214.787403] name_len 22
[ 1214.790055] 1st 16 characters of name: mkvol_bad:test_m
[ 1214.811225] ubi0 error: ubi_cdev_ioctl: bad volume creation request
[ 1214.827163] Volume creation request dump:
[ 1214.831209] vol_id 0
[ 1214.847970] alignment 1
[ 1214.850535] bytes -1
[ 1214.865295] vol_type 3
[ 1214.867860] name_len 22
[ 1214.870491] 1st 16 characters of name: mkvol_bad:test_m
[ 1214.893850] ubi0 error: ubi_cdev_ioctl: bad volume creation request
[ 1214.900146] Volume creation request dump:
[ 1214.922081] vol_id 0
[ 1214.929835] alignment 1
[ 1214.938454] bytes 0
[ 1214.941018] vol_type 3
[ 1214.954109] name_len 22
[ 1214.956762] 1st 16 characters of name: mkvol_bad:test_m
[ 1214.976558] ubi0 error: ubi_create_volume: not enough PEBs, only 1926 available
[ 1214.997017] ubi0 error: ubi_create_volume: cannot create volume 0, error -28
[ 1215.015050] ubi0 error: ubi_create_volume: not enough PEBs, only 1926 available
[ 1215.036720] ubi0 error: ubi_create_volume: cannot create volume 0, error -28
[ 1215.055972] ubi0 error: ubi_cdev_ioctl: bad volume creation request
[ 1215.073167] Volume creation request dump:
[ 1215.077213] vol_id 0
[ 1215.079754] alignment 1
[ 1215.098829] bytes 253952
[ 1215.101827] vol_type 7
[ 1215.115895] name_len 22
[ 1215.118548] 1st 16 characters of name: mkvol_bad:test_m
[ 1215.169287] ubi0 error: ubi_create_volume: volume 0 already exists
[ 1215.187754] ubi0 error: ubi_create_volume: cannot create volume 0, error -17
[ 1215.205757] ubi0 error: ubi_create_volume: volume "mkvol_bad:test_mkvol()" exists (ID 0)
[ 1215.219761] ubi0 error: ubi_create_volume: cannot create volume 1, error -17
[ 1215.287605] ubi0 error: ubi_create_volume: volume "mkvol_bad:test_mkvol()" exists (ID 0)
[ 1215.301938] ubi0 error: ubi_create_volume: cannot create volume 1, error -17
[ 1220.457401] ubi0 error: ubi_open_volume: cannot open device 0, volume 128, error -22
[ 1220.484091] ubi0 error: ubi_open_volume: cannot open device 0, volume -1, error -22
[ 1220.491845] ubi0 error: ubi_open_volume: cannot open device 0, volume 128, error -22
[ 1220.549379] ubi0 error: ubi_open_volume: cannot open device 0, volume 0, error -19
[ 1220.622112] ubi0 error: ubi_open_volume: cannot open device 0, volume 0, error -19
So I got the device to boot from SD card, and uuu created the NAND file system with U-Boot.
As long as I just read from the NAND, I am OK. I can then write, and things are still OK (using the cp command and copying from the SD card to the NAND). But if I try to read back data I have written, I get errors:
[ 848.721208] ubi0 warning: ubi_io_read: error -74 (ECC error) while reading 82 bytes from PEB 316:220808, read only 82 bytes, retry
[ 848.734112] ubi0 warning: ubi_io_read: error -74 (ECC error) while reading 82 bytes from PEB 316:220808, read only 82 bytes, retry
[ 848.752438] ubi0 warning: ubi_io_read: error -74 (ECC error) while reading 82 bytes from PEB 316:220808, read only 82 bytes, retry
[ 848.766859] ubi0 error: ubi_io_read: error -74 (ECC error) while reading 82 bytes from PEB 316:220808, read 82 bytes
[ 848.779137] CPU: 0 PID: 352 Comm: find Not tainted 5.4.24-2.1.0+gbabac008e5cf #1
[ 848.786560] Hardware name: Freescale i.MX6 Ultralite (Device Tree)
[ 848.792790] [<80111854>] (unwind_backtrace) from [<8010c3e8>] (show_stack+0x10/0x14)
[ 848.800563] [<8010c3e8>] (show_stack) from [<80c3418c>] (dump_stack+0x90/0xa4)
[ 848.807819] [<80c3418c>] (dump_stack) from [<806fdc2c>] (ubi_io_read+0x164/0x3c4)
[ 848.815334] [<806fdc2c>] (ubi_io_read) from [<806fb44c>] (ubi_eba_read_leb+0xd4/0x4fc)
[ 848.823280] [<806fb44c>] (ubi_eba_read_leb) from [<806f9ac8>] (ubi_leb_read+0x94/0x10c)
[ 848.831315] [<806f9ac8>] (ubi_leb_read) from [<803a444c>] (ubifs_leb_read+0x2c/0x78)
[ 848.839089] [<803a444c>] (ubifs_leb_read) from [<803a603c>] (ubifs_read_node+0xac/0x2a8)
[ 848.847210] [<803a603c>] (ubifs_read_node) from [<803c5c74>] (ubifs_tnc_read_node+0x5c/0x214)
[ 848.855760] [<803c5c74>] (ubifs_tnc_read_node) from [<803a7bc0>] (tnc_read_hashed_node+0x98/0x1b8)
[ 848.864743] [<803a7bc0>] (tnc_read_hashed_node) from [<803ab9a8>] (ubifs_tnc_next_ent+0x1b0/0x27c)
[ 848.873725] [<803ab9a8>] (ubifs_tnc_next_ent) from [<8039c028>] (ubifs_readdir+0x178/0x518)
[ 848.882105] [<8039c028>] (ubifs_readdir) from [<80257d24>] (iterate_dir+0x74/0x15c)
[ 848.889791] [<80257d24>] (iterate_dir) from [<80258500>] (ksys_getdents64+0x8c/0x160)
[ 848.897646] [<80258500>] (ksys_getdents64) from [<80101000>] (ret_fast_syscall+0x0/0x54)
[ 848.905748] Exception stack(0x937a7fa8 to 0x937a7ff0)
[ 848.910822] 7fa0: 00000020 024725e0 00000007 02472600 00008000 00000000
[ 848.919020] 7fc0: 00000020 024725e0 024725e4 000000d9 00000000 02472600 00000000 00454601
[ 848.927210] 7fe0: 000000d9 7edff74c 76e9d62b 76e451d6
[ 848.954326] ubi0 warning: ubi_io_read: error -74 (ECC error) while reading 67 bytes from PEB 316:237328, read only 67 bytes, retry
[ 848.972781] ubi0 warning: ubi_io_read: error -74 (ECC error) while reading 67 bytes from PEB 316:237328, read only 67 bytes, retry
[ 848.988355] ubi0 warning: ubi_io_read: error -74 (ECC error) while reading 67 bytes from PEB 316:237328, read only 67 bytes, retry
[ 849.002934] ubi0 error: ubi_io_read: error -74 (ECC error) while reading 67 bytes from PEB 316:237328, read 67 bytes
[ 849.015340] CPU: 0 PID: 352 Comm: find Not tainted 5.4.24-2.1.0+gbabac008e5cf #1
[ 849.022761] Hardware name: Freescale i.MX6 Ultralite (Device Tree)
[ 849.028993] [<80111854>] (unwind_backtrace) from [<8010c3e8>] (show_stack+0x10/0x14)
[ 849.036769] [<8010c3e8>] (show_stack) from [<80c3418c>] (dump_stack+0x90/0xa4)
[ 849.044024] [<80c3418c>] (dump_stack) from [<806fdc2c>] (ubi_io_read+0x164/0x3c4)
[ 849.051537] [<806fdc2c>] (ubi_io_read) from [<806fb44c>] (ubi_eba_read_leb+0xd4/0x4fc)
[ 849.059482] [<806fb44c>] (ubi_eba_read_leb) from [<806f9ac8>] (ubi_leb_read+0x94/0x10c)
[ 849.067518] [<806f9ac8>] (ubi_leb_read) from [<803a444c>] (ubifs_leb_read+0x2c/0x78)
[ 849.075294] [<803a444c>] (ubifs_leb_read) from [<803a603c>] (ubifs_read_node+0xac/0x2a8)
[ 849.083413] [<803a603c>] (ubifs_read_node) from [<803c5c74>] (ubifs_tnc_read_node+0x5c/0x214)
[ 849.091967] [<803c5c74>] (ubifs_tnc_read_node) from [<803a7bc0>] (tnc_read_hashed_node+0x98/0x1b8)
[ 849.100950] [<803a7bc0>] (tnc_read_hashed_node) from [<803ab9a8>] (ubifs_tnc_next_ent+0x1b0/0x27c)
[ 849.109933] [<803ab9a8>] (ubifs_tnc_next_ent) from [<8039c028>] (ubifs_readdir+0x178/0x518)
[ 849.118311] [<8039c028>] (ubifs_readdir) from [<80257d24>] (iterate_dir+0x74/0x15c)
[ 849.125994] [<80257d24>] (iterate_dir) from [<80258500>] (ksys_getdents64+0x8c/0x160)
[ 849.133850] [<80258500>] (ksys_getdents64) from [<80101000>] (ret_fast_syscall+0x0/0x54)
[ 849.141953] Exception stack(0x937a7fa8 to 0x937a7ff0)
[ 849.147027] 7fa0: 00000020 024725e0 00000007 02472600 00008000 00000000
[ 849.155225] 7fc0: 00000020 024725e0 024725e4 000000d9 00000000 02472600 00000000 00454601
[ 849.163415] 7fe0: 000000d9 7edff74c 76e9d62b 76e451d6
[ 849.177321] ubi0 warning: ubi_io_read: error -74 (ECC error) while reading 67 bytes from PEB 316:233144, read only 67 bytes, retry
[ 849.203861] ubi0 warning: ubi_io_read: error -74 (ECC error) while reading 67 bytes from PEB 316:233144, read only 67 bytes, retry
[ 849.218943] ubi0 warning: ubi_io_read: error -74 (ECC error) while reading 67 bytes from PEB 316:233144, read only 67 bytes, retry
[ 849.233214] ubi0 error: ubi_io_read: error -74 (ECC error) while reading 67 bytes from PEB 316:233144, read 67 bytes
...