Hi
A good way to have it working is adding
{
/* VGA 1024x768 65M pixel clk output */
"VGA-XGA", 60, 1024, 768, 15384,
160, 24,
29, 3,
136, 6,
0,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},
to the fb modes and set it for di1_primary.
Additionnal informations:
Boot stops here:
I/SurfaceFlinger( 2116): SurfaceFlinger is starting
I/SurfaceFlinger( 2116): SurfaceFlinger's main thread ready to run. Initializing graphics H/W...
I/imx5x.gralloc( 2116): using (fd=24)
I/imx5x.gralloc( 2116): id = DISP3 BG - DI1
I/imx5x.gralloc( 2116): xres = 1280 px
I/imx5x.gralloc( 2116): yres = 1024 px
I/imx5x.gralloc( 2116): xres_virtual = 1280 px
I/imx5x.gralloc( 2116): yres_virtual = 3072 px
I/imx5x.gralloc( 2116): bpp = 16
I/imx5x.gralloc( 2116): r = 11:5
I/imx5x.gralloc( 2116): g = 5:6
I/imx5x.gralloc( 2116): b = 0:5
I/imx5x.gralloc( 2116): width = 203 mm (160.157639 dpi)
I/imx5x.gralloc( 2116): height = 163 mm (159.568100 dpi)
I/imx5x.gralloc( 2116): refresh rate = 64.47 Hz
I/FslOverlay( 2116): overlay_device_open control pid 2116,tid 2124
I/FslOverlay( 2116): /dev/graphics/fb0 fb_var: bits_per_pixel 16,xres 1280,yres 1024,xres_virtual 1280,yres_virtual 3072
I/FslOverlay( 2116): Overlay HAL control device Created successfully
D/libEGL ( 2116): loaded /system/lib/egl/libGLES_android.so
D/libEGL ( 2116): loaded /system/lib/egl/libEGL_imx51.so
D/libEGL ( 2116): loaded /system/lib/egl/libGLESv1_CM_imx51.so
D/libEGL ( 2116): loaded /system/lib/egl/libGLESv2_imx51.so
Thks
thomas
T
Thomas Bandelier said:
HiRemi
I use this config:
setenv bootargs ${bootargs} init=/init androidboot.console=ttymxc0 di1_primary vga => did not workand as I wanted to use VGA + HDMI (2nd) I tried this one too:
setenv bootargs ${bootargs} init=/init androidboot.console=ttymxc0 di1_primary video==mxcdi0fb:RGB24,1024x768M@60 hdmi
which did not work either
I managed later to use VGA as single screen with:
setenv bootargs ${bootargs} init=/init androidboot.console=ttymxc0 di1_primary video=mxcdi1fb:GBR24,VGA-XGA vga
But I still couldn't find a way to use VGA and hdmi at the same time.
Any clue on that?
Thanks
Remi Lorriaux said:
What resolution are you using?
HiRemi
I use this config:
setenv bootargs ${bootargs} init=/init androidboot.console=ttymxc0 di1_primary vga => did not work
and as I wanted to use VGA + HDMI (2nd) I tried this one too:
setenv bootargs ${bootargs} init=/init androidboot.console=ttymxc0 di1_primary video==mxcdi0fb:RGB24,1024x768M@60 hdmi
which did not work either
I managed later to use VGA as single screen with:
setenv bootargs ${bootargs} init=/init androidboot.console=ttymxc0 di1_primary video=mxcdi1fb:GBR24,VGA-XGA vga
But I still couldn't find a way to use VGA and hdmi at the same time.
Any clue on that?
Thanks
Remi Lorriaux said:
What resolution are you using?