Adding patches to build uImage (AVB)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding patches to build uImage (AVB)

383 Views
ajayvenkatakris
Contributor II

Hi I want to build a uImage for AVB. I have found the link with the required patches needed to build the uImage. But how and where should I add these patches for building the image? Should I add it in the local.conf file and if yes, how do I add it?

0 Kudos
2 Replies

296 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ajay

please refer to yocto faq sect.2.2.2. Applying Patches

Yocto Project Linux Kernel Development Manual 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

296 Views
ajayvenkatakris
Contributor II

Hi,

   There are many bbappend files available. I am building an fsl-image-gui for imx6dl sabre auto board. At exactly which bbappend file should I add the patch files?

0 Kudos