Hi Everybody,
I have a few questions related to LINUX SPI concepts and SLAVE MODE implementations.
I am trying to port an IMX6 board to embedded linux by yocto from another operating system. Right now I need to port one SPI SLAVE MODE peripheral and one SPI MASTER MODE peripheral to port.
Linux-imx kernel version is 4.9.88. It is coming from yocto packages released by NXP.
I have added 2 spi devices using spidev userspace driver and tested with spidev_test loopback test. On loopback test it seem successful. But both are in SPI MASTR MODE.
When I checked the concepts of SPI on linux I encountered 2 nice videos on youtube
"https://www.youtube.com/watch?v=tCa_ydVwKhM&list=WL&index=3&t=0s"
"https://www.youtube.com/watch?v=MV8Sy6jGUIE&list=WL&index=2&t=0s"
First one defines slave mode support on linux and later one explains SPI subsystem on Linux kernel.
An far as I understand the SPI slave implementation is in LINUX Kernel.
Q1 Is it ready to use for an IMX6 system? If I had a newer version of kernel would it be easily implemented? Is there such an example that works for imx-yocto-bsp for imx6 SPI slave mode?
Q2 Can I port the SLAVE MODE capability from later kernels to my kernel version 4.9.88? How can i do that?
Q3 Is controller driver spi-imx.c used for this purpose? On device tree can i specify spidev as "compatible" parameter? How will spidev userspace driver use spi-imx.c as a control driver? How is the connection between protocol driver (userspace driver) and controller driver is established?
Q4 May be is it possible to change my linux-imx version to a kernel that supports spi slave mode functionality? It also needs to be supported by a yocto environment.
I know these are quite wide and unclear questions but it is so because my mind is also confused on concepts.
I hope to clarify these issues by your answers.
Best Regards
Yavuz
已解决! 转到解答。
Hi,
I have decided not to port spi slave support to an older version of kernel but rather switched to a kernel version 5.4.24.
Best Regards
Hi,
I have decided not to port spi slave support to an older version of kernel but rather switched to a kernel version 5.4.24.
Best Regards
Thank You @Yuri for your response,
I checked "https://community.nxp.com/t5/i-MX-Processors/ECSPI-slave-mode-support-for-iMX6/m-p/767130#M119124"
it is definitely the same kind of problem.
But the thread you referred do not explain how to do that?
which files are to be updated for this purpose?
and how can i test it?
Regards
It is needed to rebuild the kernel; under Yocto:
By default it is not supported; the following sequence may be performed for SPIDEV :
$ bitbake linux-imx -c menuconfig
# select DEVICE DRIVERS -> SPI Support -> User mode SPI device driver support
$ bitbake linux-imx
$ bitbake core-image-minimal