Addind New System Service to AOSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Addind New System Service to AOSP

跳至解决方案
3,866 次查看
kishorepoojari
Contributor III

Hello All ,

  I am working on IMX6 Solo light EVK Borad , whener I add new system service to the android framework (Android Lollipop 5.0.1) following error is coming and android is not booting.

Log Message:

....

....

ALSA device list:

  #0: wm8962-audio

  #1: imx-spdif

Freeing unused kernel memory: 340K (80e7b000 - 80ed0000)

type=1403 audit(1.640:2): policy loaded auid=4294967295 ses=4294967295

type=1404 audit(1.650:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295

init: /dev/hw_random not found

Console: switching to colour dummy device 80x30

init: /dev/hw_random not found

EXT4-fs (mmcblk1p5): mounted filesystem with ordered data mode. Opts: barrier=1

fs_mgr: __mount(source=/dev/block/mmcblk1p5,target=/system,type=ext4)=0

EXT4-fs (mmcblk1p4): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk1p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic

fs_mgr: __mount(source=/dev/block/mmcblk1p4,target=/data,type=ext4)=0

EXT4-fs (mmcblk1p6): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk1p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit

fs_mgr: __mount(source=/dev/block/mmcblk1p6,target=/cache,type=ext4)=0

EXT4-fs (mmcblk1p7): mounted filesystem with ordered data mode. Opts: (null)

fs_mgr: __mount(source=/dev/block/mmcblk1p7,target=/device,type=ext4)=0

binder:

err_no_context_mgr_node

binder: 116:116 transaction faileddd 29189, size 0-0

init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead

init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead

init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead

init: cannot find '/system/bin/debuggerd64', disabling 'debuggerd64'

init: cannot find '/system/bin/install-recovery.sh', disabling 'flash_recovery'

android_usb: already disabled

read descriptors

read strings

mtp_bind_config

android_work: sent uevent USB_STATE=CONNECTED

android_work: sent uevent USB_STATE=DISCONNECTED

android_usb gadget: high-speed config #1: android

android_work: sent uevent USB_STATE=CONFIGURED

healthd: BatteryTemperaturePath not found

healthd: BatteryTechnologyPath not found

csi_v4l_open: Internal error, camera is not found!

csi_v4l_open: Internal error, camera is not found!

warning: `main' uses 32-bit capabilities (legacy support in use)

request_suspend_state: wakeup (3->0) at 47887247671 (1970-01-01 00:00:46.238294463 UTC)

lowmemorykiller: lowmem_shrink: convert oom_adj to oom_score_adj:

lowmemorykiller: oom_adj 0 => oom_score_adj 0

lowmemorykiller: oom_adj 1 => oom_score_adj 58

lowmemorykiller: oom_adj 2 => oom_score_adj 117

lowmemorykiller: oom_adj 3 => oom_score_adj 176

lowmemorykiller: oom_adj 9 => oom_score_adj 529

lowmemorykiller: oom_adj 15 => oom_score_adj 1000

binder: undelivered transaction 17836

alarm_release: clear alarm, pending 0

binder: 120:213 transaction faileddd 29189, size 68-0

request_suspend_state: wakeup (0->0) at 200971899606 (1970-01-01 00:03:19.322946606 UTC)

csi_v4l_open: Internal error, camera is not found!

csi_v4l_open: Internal error, camera is not found!

request_suspend_state: wakeup (0->0) at 218105294358 (1970-01-01 00:03:36.456341233 UTC)

lowmemorykiller: lowmem_shrink: convert oom_adj to oom_score_adj:

lowmemorykiller: oom_adj 0 => oom_score_adj 0

lowmemorykiller: oom_adj 1 => oom_score_adj 58

lowmemorykiller: oom_adj 2 => oom_score_adj 117

lowmemorykiller: oom_adj 3 => oom_score_adj 176

lowmemorykiller: oom_adj 9 => oom_score_adj 529

lowmemorykiller: oom_adj 15 => oom_score_adj 1000

binder: 120:214 transaction faileddd 29189, size 68-0

alarm_release: clear alarm, pending 0

request_suspend_state: wakeup (0->0) at 229731951735 (1970-01-01 00:03:48.082998610 UTC)

csi_v4l_open: Internal error, camera is not found!

csi_v4l_open: Internal error, camera is not found!

request_suspend_state: wakeup (0->0) at 246836643778 (1970-01-01 00:04:05.187690695 UTC)

lowmemorykiller: lowmem_shrink: convert oom_adj to oom_score_adj:

lowmemorykiller: oom_adj 0 => oom_score_adj 0

lowmemorykiller: oom_adj 1 => oom_score_adj 58

lowmemorykiller: oom_adj 2 => oom_score_adj 117

lowmemorykiller: oom_adj 3 => oom_score_adj 176

lowmemorykiller: oom_adj 9 => oom_score_adj 529

lowmemorykiller: oom_adj 15 => oom_score_adj 1000

binder: undelivered transaction 24411

alarm_release: clear alarm, pending 0

binder: 120:214 transaction faileddd 29189, size 68-0

request_suspend_state: wakeup (0->0) at 258011735363 (1970-01-01 00:04:16.362781905 UTC)

csi_v4l_open: Internal error, camera is not found!

csi_v4l_open: Internal error, camera is not found!

request_suspend_state: wakeup (0->0) at 275193878365 (1970-01-01 00:04:33.544925199 UTC)

lowmemorykiller: lowmem_shrink: convert oom_adj to oom_score_adj:

lowmemorykiller: oom_adj 0 => oom_score_adj 0

lowmemorykiller: oom_adj 1 => oom_score_adj 58

lowmemorykiller: oom_adj 2 => oom_score_adj 117

lowmemorykiller: oom_adj 3 => oom_score_adj 176

lowmemorykiller: oom_adj 9 => oom_score_adj 529

lowmemorykiller: oom_adj 15 => oom_score_adj 1000

alarm_release: clear alarm, pending 0

binder: 120:214 transaction faileddd 29189, size 68-0

request_suspend_state: wakeup (0->0) at 286352135241 (1970-01-01 00:04:44.703182033 UTC)

csi_v4l_open: Internal error, camera is not found!

csi_v4l_open: Internal error, camera is not found!

Please help me sort out this issue...

Regards,

Kishore P

标签 (4)
标记 (2)
1 解答
2,301 次查看
gary_bisson
Senior Contributor III

Hi Kishore,

It means your SystemServer is crashing during its initialization, most likely due to your custom system service.

Please check your logcat, it will hopefully give you more information.

Regards,

Gary

在原帖中查看解决方案

3 回复数
2,302 次查看
gary_bisson
Senior Contributor III

Hi Kishore,

It means your SystemServer is crashing during its initialization, most likely due to your custom system service.

Please check your logcat, it will hopefully give you more information.

Regards,

Gary

2,301 次查看
gusarambula
NXP TechSupport
NXP TechSupport

You did not include more details on which service you're adding but I would suggest maybe looking at the Android Developer Forums on the specifics of the kind of service you're adding. You're also welcome to add it here so other community users may contribute.

0 项奖励
回复
2,301 次查看
kishorepoojari
Contributor III

Hello Gary,

   I followed the following Blog to add new custom System Service to the AOSP (Lollipop 5.0.2).

shridutt kothari's blog: Adding New System Service in Android

Android-Adding SystemService - Texas Instruments Wiki

After adding new System Service , we have to add the Service to  /external/sepolicy/service_contexts to avoid SELinux policy denies

refer the below post

http://stackoverflow.com/questions/30165852/selinux-permission-denied-for-a-new-framework-service-in... .

Regards,

Kishore P

0 项奖励
回复