After setup FBTFT Driver (SSD1351) for my WARP7
Now I want to test my framebuffer to display something on screen.
All resources refer to con2fbmap. but it seem to be only existed in RPi.
How can I add con2fbmap to my Yocto image ? (I'm using core-image-base image)
Note: I searched for packages that can be added to yocto here OpenEmbedded Layer Index - meta-fsl-demos
But it do not have fbset package
解決済! 解決策の投稿を見る。
Have you tried to run : bitbake fbset ?
Otherwise, you can add the following command to local.conf and rebuild your image.
IMAGE_INSTALL_append += " fbset"
BR
PJ
Sorry for my naive question, but....How can i use it ?
Have you tried to run : bitbake fbset ?
Otherwise, you can add the following command to local.conf and rebuild your image.
IMAGE_INSTALL_append += " fbset"
BR
PJ
Just adding to PJ's answer, you can see if the fbset recipe is available on your bitbake environment by running:
$ bitbake -s | grep fbset
Regards,
Otherwise, you can add the following command to local.conf and rebuild your image.
IMAGE_INSTALL_append += " fbset"
Thank you for your time, guys. I will take this answer :smileyhappy:
Hi chaunguyenngoc
You can find fbset into the meta-openembedded layer (meta-openembedded/meta-oe/recipes-support/fbset at master · openembedded/meta-openembedded · GitHub ) (Already in bitbake's configuration (bblayer.conf))
BR
PJ