We have attached ar1021 i2c touch controller to our product which uses Kontron SMARC Soc. How can I define it in device tree?
ar1021 i2c touch controller's interrupt line is connected to the pin P109 which is defined in 'SMARC sMAX6i' manual as
Pin | Signal | Direction | Termination | Type/tol | Controller | Controller PIn name | Port dl | Port solo | iomux instance |
---|---|---|---|---|---|---|---|---|---|
P109 | GPIO1 / CAM1_PWR# | Bi-Dir | PU-470k | CMOS / VDD_IO | iMX6 | EIM_DA1 | GPIO3_IO01 | GPIO3_IO01 | ALT5 / ALT5 |
I have tried define ar1021 in device tree as below. Driver loads proberly but interrupt callback function is never called.
&i2c3 | { |
status = "okay"; |
ar1021@4D { | |||||||
compatible = "microchip,ar1021-i2c"; | |||||||
reg = <0x4D>; | |||||||
interrupt-parent = <&gpio3>; | |||||||
interrupts = <1 IRQ_TYPE_EDGE_FALLING>; | |||||||
wakeup-gpios = <&gpio3 1 IRQ_TYPE_LEVEL_HIGH>; |
}; |
};
Problem seems to be that interrupt for PIN P109 is not defined correctly. Any ideas?
Hi Ari
please look at similar example for eGalax touch controller
http://lists.infradead.org/pipermail/linux-arm-kernel/2012-August/113944.html
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------