Accuracy of i.MX6DQ timers.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Accuracy of i.MX6DQ timers.

跳至解决方案
644 次查看
satoshishimoda
Senior Contributor I

Hi community,

Our customer have a question about i.MX6DQ.

They want to know the accuracy of each i.MX6DQ timers (GPT, EPIT, SRTC, ・・・).

Would you let me know it?

(e.g. GPT accuracy = PLL accuracy = 24MHz crystal accuracy, SRTC accuracy = 32kHz crystal accuracy)

Best Regards,

Satoshi Shimoda

标签 (4)
标记 (1)
0 项奖励
回复
1 解答
543 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Accuracy of the mentioned timers also are affected by parameters of internal PLLs, which, strictly speaking, are not specified. In particular, we can refer to Table 2-20 (24 MHz crystal tolerance guidelines) of Hardware Development Guide for i.MX 6 , assuming stability (thermal, voltage and other) of PLL output clock is fully defined by external crystal / oscillator, and i.MX6 meets USB, PCIe, Ethernet clock specs. 

< http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf >

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
544 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Accuracy of the mentioned timers also are affected by parameters of internal PLLs, which, strictly speaking, are not specified. In particular, we can refer to Table 2-20 (24 MHz crystal tolerance guidelines) of Hardware Development Guide for i.MX 6 , assuming stability (thermal, voltage and other) of PLL output clock is fully defined by external crystal / oscillator, and i.MX6 meets USB, PCIe, Ethernet clock specs. 

< http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf >

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复