Accessing SDIO pins in MCIMX28EVKJ: i.MX28 Evaluation Kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Accessing SDIO pins in MCIMX28EVKJ: i.MX28 Evaluation Kit

ソリューションへジャンプ
817件の閲覧回数
ganeshh
Contributor III

Hi,

I am planning to buy MCIMX28EVKJ: i.MX28 Evaluation Kit. in hardware schematics SDIO pins are shown but in evaluation kit no headers are given so is it just the sd card slot or pins available . i want to interface a wifi module so sdio pins are needed.

ラベル(2)
0 件の賞賛
1 解決策
694件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ganesh, i.MX28 EVK schematic p.8 shows

SD interface. SDIO interface uses the same pins, i.MX28

has SSP module and it is used for both SD/SDIO.

Actually there is no difference between SD and SDIO signals.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
695件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ganesh, i.MX28 EVK schematic p.8 shows

SD interface. SDIO interface uses the same pins, i.MX28

has SSP module and it is used for both SD/SDIO.

Actually there is no difference between SD and SDIO signals.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛