About the minimum clock frequency of the core for i.MX6 Solo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the minimum clock frequency of the core for i.MX6 Solo

ソリューションへジャンプ
2,256件の閲覧回数
yuuki
Senior Contributor II

Dear all,

Would you teach about the minimum clock frequency of the core for i.MX6 Solo?

According to the "Table 9. Operating Ranges" of a datasheet, the following is indicated.
- Run mode: LDO enabled => VDD_ARM_IN : 1.175-1.5V "LDO Output Set Point (VDD_ARM_CAP) = 1.05 V minimum for operation up to 396 MHz."
- Run mode: LDO bypassed => VDD_ARM_IN : 1.05-1.3V "LDO bypassed for operation up to 396 MHz"

However, the minimum is not shown.

Would you teach the minimum CPU Core clock frequency in which the system can operate?

Best Regards,

ラベル(1)
0 件の賞賛
返信
1 解決策
1,807件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Yuuki

     The CPU freq should can be lower, but I am not sure whether the voltage can be lower, I believe it can NOT be lower, but you had better to confirm with someone who is more familiar with it, as far as I know, for solo, the CACHE power is coming from VDDARM, and the CACHE's voltage can NOT be too low.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,807件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, yuuki

     May I know why you want the minimum cpu core clock freq? In datasheet, the lowest setpoint is 396MHz, even you run cpu at a lower freq, you still need to use the voltage of 1.05V. And with same voltage, the higher freq cpu runs, the more power it saves, as CPU can enter idle longer. So, with 1.05V, CPU run at 396MHz can save more power than running at freq lower than 396MHz.

1,807件の閲覧回数
yuuki
Senior Contributor II

Dear Yongcai Huang-san,

Thank you for the reply.

I target lower power consumption.

"So, with 1.05V, CPU run at 396MHz can save more power than running at freq lower than 396MHz."
I am also the same understanding as you.

I would like to know the lower limit of voltage and frequency.

May I have advice?

Best Regards,
Yuuki

0 件の賞賛
返信
1,808件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Yuuki

     The CPU freq should can be lower, but I am not sure whether the voltage can be lower, I believe it can NOT be lower, but you had better to confirm with someone who is more familiar with it, as far as I know, for solo, the CACHE power is coming from VDDARM, and the CACHE's voltage can NOT be too low.

0 件の賞賛
返信