Dear All,
We want to use PCIe on original OS.
The setting value is investigated by dump registers on Linux.
RM has the following descriptions about the switching of RC and EP.
Page 2052 in Applications Processor Reference Manual (Document Number: IMX6SDLRM Rev. 1, 04/2013) :
Section 37.4.13 GPR12 (IOMUXC_GPR12)
Address: 20E_0000h base + 30h offset = 20E_0030h
Field : 15-12 DEVICE_TYPE
Description :
PCIe_CTL - Device/Port Type. Indicates the specific type of
this PCI Express Function (EP or RC)
DEVICE_TYPE field values 0011-1111 are reserved.
However, the dump value was "0100"
root@wandboard:~# lspci
00:00.0 PCI bridge: Device 16c3:abcd (rev 01)
01:00.0 PCI bridge: Texas Instruments XIO2001 PCI Express-to-PCI Bridge
02:00.0 RAM memory: XXXXXXXXXXXXXXXXXXXXXXXXXXXXX. Device 8002 (rev 01)
root@wandboard:/# ./unit_tests/memtool 20E0030 10
E
Reading 0x10 count starting at address 0x020E0030
0x020E0030: 0F004490 0593A046 00000000 00000000
0x020E0040: 00000000 00000000 00000000 00000003
0x020E0050: 00000003 00000005 00000005 00000005
0x020E0060: 00000005 00000005 00000005 00000005
root@wandboard:~#
Please let me know what kind of meaning this value has.
Best Regard,
George
已解决! 转到解答。
• 0000b: PCI Express Endpoint device
• 0001b: Legacy PCI Express Endpoint device
• 0100b: Root Port of PCI Express Root Complex
Device_type 0100b causes the DM core to operate in RC mode.
You can check page 4198 line 1-2 on sdl rm:
The core is not in RC mode (applies to DM product only).
That is, device_type[3:0] is not 4'b0100.
• 0000b: PCI Express Endpoint device
• 0001b: Legacy PCI Express Endpoint device
• 0100b: Root Port of PCI Express Root Complex
Device_type 0100b causes the DM core to operate in RC mode.
You can check page 4198 line 1-2 on sdl rm:
The core is not in RC mode (applies to DM product only).
That is, device_type[3:0] is not 4'b0100.