About the ECSPI Master Mode Timing Parameters.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the ECSPI Master Mode Timing Parameters.

Jump to solution
1,049 Views
takashitakahash
Contributor III

Hi community.

Our customer has two question below.

About the ECSPI Master Mode Timing Parameters.

1, "ECSPIx_SCLK High or Low Time (tSW)"

Read at the time of 21.5ns (min) it is would be fixedregardless of the setting frequency of ECSPIx_SCLK?

(If the slower the frequency of SCLK when tSW (min) will also be larger? )

2 "ECSPIx_MISO Setup Time (tSmiso)"

Read at: tSW=21.5ns(min), tSmiso 18 ns (min) seems like a tough value  and nalow is it correct?

Labels (1)
0 Kudos
Reply
1 Solution
903 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

1. Read time of 21.5ns (min) is not fixed, it is given for max.

available frequency and will be increased proportionally ECSPIx_SCLK frequency

2. you are right, it seems as tough at max. frequency, however ar lower

frequency this may be acceptable

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
903 Views
takashitakahash
Contributor III

Hi commujnity.

I want to make sure about the answer.

About for 1.

tSW (min) is change by setting frequency, numerical value can be calculated from the set frequency?

(50% of the set frequency cycle?)

Example) tSW value, when it is set to ECSPIx_SCLK = 20MHz (min)

And about for 2.

Please allowed to check just in case.

tSmiso is fixed min = 18ns, regardless of the setting frequency.

0 Kudos
Reply
903 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

tSW=21.5ns (min) is defined by max. operational frequency.

With 20MHz it will be T/2 (T=1/20MHz)   (typ.)

yes, min = 18ns, regardless of the setting frequency

~igor

904 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

1. Read time of 21.5ns (min) is not fixed, it is given for max.

available frequency and will be increased proportionally ECSPIx_SCLK frequency

2. you are right, it seems as tough at max. frequency, however ar lower

frequency this may be acceptable

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply