About tearing issue with OpenGL + X11 in i.MX6DQ.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About tearing issue with OpenGL + X11 in i.MX6DQ.

跳至解决方案
1,028 次查看
keitanagashima
Senior Contributor I

Dear All,

Hello. I have a question about tearing issue with OpenGL + X11 in i.MX6DQ.

BSP : L3.14.28_1.0.0

Environment : OpenGL + X11

[Issue]

The tearing occurs when waiting for VSYNC and displaying.

  #define MXCFB_WAIT_FOR_VSYNC    _IOW('F', 0x20, u_int32_t)

  ioctl(fd_, MXCFB_WAIT_FOR_VSYNC, 0);

This Phenomenon looks below issue.

Refer to 6.1.7  Tearing in i.MX 6 Graphics User’s Guide, Rev. 0, 12/2015

There is description of "This tearing free feature will be described in next release.".

But, the below information seem to already fix this issue.

See Comment 4.

https://bugzilla.yoctoproject.org/show_bug.cgi?id=6760

[Question]

When is this tearing issue fixed?

(Or, which BSP version was it fixed?)

Best regards,

Keita

标签 (4)
0 项奖励
回复
1 解答
646 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Keita,

Tearing is a known X11 problem, in fact it is an X11 architecture problem. So far there is no any official fix for X11 tearing issue with vsync, however several gpu bug fixed have been added to 3.14.28-1.0.1 patch such as: gitorious.org Git - efikamx:linux-kernel.git/commit  using export FB_MULTIBUFFER option, however X11 EGL is single buffered and there is no support for VSYNC.

Please check the 3.14.28-1.0.1 patch release notes for more information

http://www.nxp.com/files/32bit/doc/support_info/IMX6L31428101RN.pdf

Regards

在原帖中查看解决方案

0 项奖励
回复
1 回复
647 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Keita,

Tearing is a known X11 problem, in fact it is an X11 architecture problem. So far there is no any official fix for X11 tearing issue with vsync, however several gpu bug fixed have been added to 3.14.28-1.0.1 patch such as: gitorious.org Git - efikamx:linux-kernel.git/commit  using export FB_MULTIBUFFER option, however X11 EGL is single buffered and there is no support for VSYNC.

Please check the 3.14.28-1.0.1 patch release notes for more information

http://www.nxp.com/files/32bit/doc/support_info/IMX6L31428101RN.pdf

Regards

0 项奖励
回复