Dear All,
In FSL WindowsBSP,
We have the problem that a CPU may be hung-up, when a register is written by USB Driver.
When a USB driver writes any value into offset 0x017C of HS-USB register, this problem may occur.
In the source code of WinCE BSP, this register is defined as ENDPTNAKEN.
However, in a reference manual, this 0x017C register is "reserved".
MCIMX51 Multimedia Applications Processor Reference Manual Rev. 1 2/2010
- Table 60-28. HS-USB Register Summary(P.2882)
In Linux BSP source code, this 0x017C register is not defined.
In WinCE,
What kind of function does this 0x017C register have?
Is access(writing) to this 0x017C register required?
Best Regards,
Yuuki
解決済! 解決策の投稿を見る。
Hi yuuki
please look below for description,
I think its usage is optional
Best regards
igor
Dear Igor-san,
Thank you for your support.
Are there any limitations about writing in these fields?
If access to this register is deleted, does a problem occur?
We want to know how to prevent the hang-up of CPU.
Best Regards,
Yuuki
Hi yuuki
access to this register is performed in
..COMMON_FSL_V2/USBD/COMMON/pdd.c
do you mean that this piece of code is not working ?
Also this register is defined in i.MX53 RM IMX53RM
sect.77.6.30 Endpoint Nake Enable (USB_UOG_ENDPTNAKEN)
Best regards
igor
Dear Igor-san,
Thank you for your support.
> do you mean that this piece of code is not working ?
=>
No.
When it is accessed this register, a CPU may be hung up.
We are looking for this root cause and workaround.
Best Regards,
Yuuki
Hi yuuki
I think answer depends on what do you mean
by "accessed this register" - what method are you using.
Since USB driver is high speed driver, accessing its registers
as not allowed at runtime - this violates USB driver timings, they have
strict timing constraints.
I think you can write own standalone code (without OS) like
On-Board Diagnostic Suit for the i.MX53 Quick Start Board
and try to access these registers.
~igor
Dear Igor-san,
Thank you for your support.
> I think answer depends on what do you mean
> by "accessed this register" - what method are you using.
=>
The driver in FSL_WinCE6.0 BSP for i.MX51EVK has accessed to the register.
Does standalone code for i.MX51EVK exist?
Would you send it, if you have it?
Best Regards,
Yuuki
Hi yuuki
sorry, there is no official standalone code for i.MX51EVK
but you can request unofficial creatng SR ticket.
~igor