Hello,community
Is it possible to check the interrupt status with GPIO interrupt status register (GPIOx_ISR) for both Active HIGH Interrupt from INT7 from GPIO and Combined interrupt indication for GPIO1 signal 0 throughout 15?
Is Active HIGH Interrupt from INT7 from GPIO's Active HIGH high-level sensitive, not rising-edge sensitive?
Is Active HIGH Interrupt from INT7 from GPIO enabled by GPIO interrupt mask register (GPIOx_IMR)?
Best Regards, Goto
Hi Goto
>Is it possible to check the interrupt status with GPIO interrupt status register (GPIOx_ISR) for both Active HIGH >Interrupt from INT7 from GPIO and Combined interrupt indication for GPIO1 signal 0 throughout 15?
yes
>Is Active HIGH Interrupt from INT7 from GPIO's Active HIGH high-level sensitive, not rising-edge sensitive?
yes
>Is Active HIGH Interrupt from INT7 from GPIO enabled by GPIO interrupt mask register (GPIOx_IMR)?
Interrupt is configured using GPIOx_ICR1, in the same way as for other interrupts (for example Combined interrupt).
It can be masked by GPIOx_IMR.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------