About input voltage of VDD_SNVS_IN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About input voltage of VDD_SNVS_IN

790件の閲覧回数
okamotosatoshi
Contributor IV

I want to check for VDD_SNVS_IN using a coin battery.

During normal operation, VDD_SNVS_IN is the operating range is 2.9V ~ 3.3V.

- i.MX 6Solo/6DualLite Applications Processors for Consumer Products, Rev. 5 4.1.3 Operating Ranges

As an example, it shows the discharge characteristic graph of the ML621.

Immediately, coin battery is reduced to about 2.5V.

In addition, less than the operating range and supplies using the PMIC (MMPFxxxx).

ML621_Discharge.png

If you want to back up the RTC in the Coin Cell Mode, operating  range of VDD_SNVS_IN will be 2.9V ~ 3.3V?

Regards,

-satoshi

ラベル(2)
0 件の賞賛
4 返答(返信)

608件の閲覧回数
okamotosatoshi
Contributor IV

Hi, Yuri

Thank you for answering.

I consider the configuration of the backup circuit.

It became the future of help.

Regards,

-satoshi

0 件の賞賛

608件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Strictly speaking, You are right, VDD_SNVS_IN operating range from 2.9 V  provides

difficulties for battery selection and using, when we should take into account battery

discharging. Nevertheless, the value of 2.9 V is correct. 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

608件の閲覧回数
okamotosatoshi
Contributor IV

Hi, Yuri

Thank you for answering.

It may be difficult itself to back up the RTC(in IMX) in the coin battery.

I want you to presentation if there is a reference circuit of the RTC backup.

(Reference circuit you do not want to use the PMIC.)

Regards,

-satoshi

0 件の賞賛

608件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello, Satoshi !

     SABRE SD Board / Platform design may be used as reference, but

it is based on PMIC. No i.MX6 designs without PMIC from NXP.
Basically it is possible to connect i.MX6 VDD_SNVS_IN with a battery directly.

Regards,
Yuri.

0 件の賞賛