About i.MX6Q with USB & LAN PHY in deep sleep mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About i.MX6Q with USB & LAN PHY in deep sleep mode

Jump to solution
712 Views
keitanagashima
Senior Contributor I

Dear All,

Hello.

I have questions about i.MX6Q in deep sleep mode.

Refer to Table 10-1. Aimed power modes in IMX6DQRM(Rev.2).

There is below description.

"Interrupts from modules those could generate asynchronous interrupts (Keypad, GPIO, SNVS)".

[Q1]

Can i.MX6 return (resume) from deep sleep mode by detection of VBUS with USB?

[Q2]

When entering a sleep-mode, does it make LAN PHY a sleep-mode, too?

(I consider that LAN PHY enters a sleep-mode because the current consumption of LAN_PHY decreased in Sleep Mode.)

Best Regards,

Keita

Labels (4)
0 Kudos
1 Solution
531 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

1. yes

VBUS.jpg

2. yes if used LAN PHY supports such sleep-mode, this may depend

on PHY chip.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
532 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

1. yes

VBUS.jpg

2. yes if used LAN PHY supports such sleep-mode, this may depend

on PHY chip.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
531 Views
keitanagashima
Senior Contributor I

Hi Igor,

Thank you for your reply.

I tried to test by below command with L3.14.28_1.0.0.

====

echo enabled > /sys/bus/platform/devices/20c9000.usbphy/power/wakeup

echo enabled > /sys/bus/platform/devices/2184000.usb/power/wakeup

echo enabled > /sys/bus/platform/devices/ci_hdrc.0/power/wakeup

echo enabled > /sys/bus/usb/devices/usb1/power/wakeup

====

And, I confirmed USB wake up.

Thank you!

Best Regards,

Keita

0 Kudos