About changing the internal LDOs voltage in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About changing the internal LDOs voltage in i.MX6DQ.

Jump to solution
2,200 Views
keitanagashima
Senior Contributor I

Dear All,

Hello. We'd like to change the internal LDOs voltage.

Could you tell me the way of proper setting about below LDOs?

(We'd like to know the setting in u-boot and kernel.)

OS: jb4.2.2_1.1.0

[LDO's output voltage]

- LDO_SOC (VDD_SOC_CAP) : 1.275V   //for DDR clock Jitter

- LDO_ARM (VDD_ARM_CAP) : 1.250V   //for ARM freq up (1GHz)

- LDO_PU (VDD_PU_CAP) : 1.275V   //for VPU freq up (352MHz)

- LDO1P1 (NVCC_PLL_OUT) : 1.175V   //for DDR clock Jitter

- LDO2P5 (VDD_HIGH_CAP)  : 2.700V    //for DDR clock Jitter

[Other information]

> ARM freq up (1GHz)

Change the ARM clock

$ echo userspace > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor

$ echo 996000 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed

> VPU freq up (352MHz)

Add the kernel config (menu config)

  [*] MX6 VPU 352MHz

Best Regards,

Keita

Labels (4)
0 Kudos
1 Solution
1,400 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Keita

[Q1] Should one change below setting to change the LDO voltage?

[Q2] Is there a code which it should set to the others?

     (We worry about whether or not a overwritten by other codes.)

For Kernel;

Change the "cpu_op" voltage in arch\arm\mach-mx6\cpu_op-mx6.c.

[Anson] Correct, after kernel boot up, only cpufreq will change the voltage/freq, it will follow the table in the file you listed, you just need to change the table accordingly, choose the right array.

For U-boot;

Change the "arch_cpu_init" in cpu\arm_cortexa8\mx6\generic.c

[Anson] Yes, but the setting in u-boot will be over written by kernel cpufreq driver if it is enabled after kernel boot up. CPUFreq is the only one who change the voltage/freq.

View solution in original post

7 Replies
1,400 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Keita

     Please try below:

[LDO's output voltage]

- LDO_SOC (VDD_SOC_CAP) : 1.275V   //for DDR clock Jitter

- LDO_ARM (VDD_ARM_CAP) : 1.250V   //for ARM freq up (1GHz)

- LDO_PU (VDD_PU_CAP) : 1.275V   //for VPU freq up (352MHz)

[Anson] no need to do changes, LDO_PU always equal to LDO_SOC. BTW, to use LDO enable mode, you have to use imx6q-sabresd-ldo.dtb, by default we use ldo bypass mode which is using imx6q-sabresd.dtb, for SabreAI board, only LDO enable mode is supported, no need to change dtb. Please do it according to your board design.

- LDO1P1 (NVCC_PLL_OUT) : 1.175V   //for DDR clock Jitter

[Anson] LDO1P1 is NOT dynamically changed in kernel, we use default value which is 1.1V, if you want to increase it to 1.175V, you need to program PMU_REG_1P1 register in PMU chapter, bit [12:8] need to modified to 0x13, you can do it in uboot using "md/mw" command to read/write register or using /unit_tests/memtool to read/write register in kernel. Or you can add code in uboot to do this change, either way is OK.

- LDO2P5 (VDD_HIGH_CAP)  : 2.700V    //for DDR clock Jitter

[Anson] Same as above, modify the PMU_REG_2P5 bit [12:8] to 0x18, 0x10 means 2.5V, each step is 25mV, so add 8 steps to make it 2.7V.

[Other information]

> ARM freq up (1GHz)

Change the ARM clock

$ echo userspace > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor

$ echo 996000 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed

[Anson] for 1GHz, the voltage we used for VDD_SOC/PU_CAP is 1.25V, to increase them to 1.275V, you need to modify the table in arch/arm/boot/dts/imx6q.dtsi,

29                         operating-points = <

30                                 /* kHz    uV */

31                                 1200000 1275000

32                                 996000  1250000

33                                 852000  1250000

34                                 792000  1175000

35                                 396000  975000

36                         >;

37                         fsl,soc-operating-points = <

38                                 /* ARM kHz  SOC-PU uV */

39                                 1200000 1275000

40                                 996000  1250000     /* change to 1275000 */

41                                 852000  1250000

42                                 792000  1175000

43                                 396000  1175000

44                         >;

> VPU freq up (352MHz)

Add the kernel config (menu config)

  [*] MX6 VPU 352MHz

[Anson] Correct.

1,400 Views
keitanagashima
Senior Contributor I

Dear Yongcai Huang,

Hello. Thank you for your great answer!

But, my customer is using b4.2.2_1.1.0 and Kernel 3.0.35.

So, the .dtb file doesn't exist...

Best Regards,

Keita

0 Kudos
1,400 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Keita

     OK, if for kernel 3.0.35, by default kernel uses LDO bypass mode, to use LDO enable mode, you have to add "ldo_active=on" in u-boot cmdline, then kernel will switch to LDO enable mode, otherwise, internal VDDARM and VDDSOC/PU's LDO will be bypass, to adjust their voltage, you have to adjust external PMIC's output.

0 Kudos
1,400 Views
keitanagashima
Senior Contributor I

Dear Yongcai Huang,

Hello. Sorry for my delay response.

My customer isn't use the PMIC (They are using discreet ICs).

Because they aren't using "arch\arm\mach-mx6\mx6q_sabresd_pmic_pfuze100.c", LDO is enabled.

When LDO is enabled, is it right in the below my understanding?

PLease check it.

[Q1] Should one change below setting to change the LDO voltage?

[Q2] Is there a code which it should set to the others?

     (We worry about whether or not a overwritten by other codes.)

For Kernel;

Change the "cpu_op" voltage in arch\arm\mach-mx6\cpu_op-mx6.c.

For U-boot;

Change the "arch_cpu_init" in cpu\arm_cortexa8\mx6\generic.c

Best Regards,
Keita

0 Kudos
1,401 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Keita

[Q1] Should one change below setting to change the LDO voltage?

[Q2] Is there a code which it should set to the others?

     (We worry about whether or not a overwritten by other codes.)

For Kernel;

Change the "cpu_op" voltage in arch\arm\mach-mx6\cpu_op-mx6.c.

[Anson] Correct, after kernel boot up, only cpufreq will change the voltage/freq, it will follow the table in the file you listed, you just need to change the table accordingly, choose the right array.

For U-boot;

Change the "arch_cpu_init" in cpu\arm_cortexa8\mx6\generic.c

[Anson] Yes, but the setting in u-boot will be over written by kernel cpufreq driver if it is enabled after kernel boot up. CPUFreq is the only one who change the voltage/freq.

1,400 Views
keitanagashima
Senior Contributor I

Hi Yongcai,

Great answer!

Thank you very much!!

Best Regards,

Keita

0 Kudos
1,400 Views
karina_valencia
NXP Apps Support
NXP Apps Support

AnsonHuang​ please continue with the  follow up

0 Kudos