Dear all,
We use Linux L3 .10.53 BSP on i.MX6DualLite.
When Video Playback is run in succession by using Gstreamer, the following error occurs.
==================================================================================
GLib-GObject-CRITICAL **: g_object_ref: assertion 'object->ref_count > 0' failed
GStreamer-CRITICAL **: gst_bin_iterate_elements: assertion 'GST_IS_BIN (bin)' failed
GStreamer-CRITICAL **: gst_iterator_filter: assertion 'it != NULL' failed
GLib-GObject-CRITICAL **: g_object_unref: assertion 'G_IS_OBJECT (object)' failed
GStreamer-CRITICAL **: gst_iterator_next: assertion 'it != NULL' failed
GLib-GObject-CRITICAL **: g_value_unset: assertion 'G_IS_VALUE (value)' failed
GStreamer-CRITICAL **: gst_iterator_free: assertion 'it != NULL' failed
GStreamer-CRITICAL **: gst_element_iterate_src_pads: assertion 'GST_IS_ELEMENT (element)' failed
GStreamer-CRITICAL **: gst_iterator_next: assertion 'it != NULL' failed
GLib-GObject-CRITICAL **: g_value_unset: assertion 'G_IS_VALUE (value)' failed
GStreamer-CRITICAL **: gst_iterator_free: assertion 'it != NULL' failed
==================================================================================
We found a following thread of Community.
https://community.nxp.com/thread/357567
According to these contents, I seem that Gstreamer version 1.4 has a problem.
(There is the same problem with Gstreamer ver1.2 of L3.10.53.)
" For long time video playback, ..."
On the other hand, In Gstreamer version 1.8 of L4.1.15, this description is deleted.
<Questions>
- Is there the detailed information about the modified contents of this part?
- Is there the method to port this modified point to Gstreamer version 1.4(or version 1.2)?
May I have any advice?
Best Regards,
Yuuki
解決済! 解決策の投稿を見る。
I dont' have detailed information about this issue, in the old bsp, if runing more than 12 hours, maybe cased some random issue, for install new gstreamer I send the link to you for reference, you can refer to it to install new gstreamer
GStreamer-devel - How do I install Gstreamer 1.8.3 under Ubuntu 14.04?
I dont' have detailed information about this issue, in the old bsp, if runing more than 12 hours, maybe cased some random issue, for install new gstreamer I send the link to you for reference, you can refer to it to install new gstreamer
GStreamer-devel - How do I install Gstreamer 1.8.3 under Ubuntu 14.04?
Dear Joan-san,
Thank you for your support.
The cause was mismatched for a state of Gstreamer.
We were able to evade a problem by modifying application.
Best Regards,
Yuuki