I'm new to Yocto development for the NXP i.MX boards,
I am using the following command to build the YOCTO environment.There are no flash files in the tmp/deploy/images/imx8mp lpddr4 evk/ folder, but they were available when I built with imx-5.10.35-2.0.0.xml before. Why is this? Can you help me build YOCTO correctly?
mkdir imx-yocto-bsp
cd imx-yocto-bsp
repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-mickledore -m imx-6.1.22-2.0.0.xml
repo sync
DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build
bitbake imx-image-full -c populate_sdk
Hi @LDX
The "populate_sdk" generates a development SDK which mainly includes the tools, toolchain.
As you have finished the bitbake imx-image-full -c populate_sdk, just to run bitbake imx-image-full then to get the flash file that you need.
It won't take much time.
Best regards
Harvey