About WMA10 Std decoder in KK4.4.3_2.0.0 with i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About WMA10 Std decoder in KK4.4.3_2.0.0 with i.MX6DQ.

Jump to solution
1,190 Views
keitanagashima
Senior Contributor I

Dear All,

Hello. 

Refer to 5.4 Audio decoder in "i.MX Android Extended Codec Release Note" of Rev KK4.4.3_2.0.0-ga.

There is description of "WMA10 Std".

But, we think that "WMA10 Std" doesn't exist. (Only existing the WMA10 Pro.)

Does "WMA10 Std" exist?

Best Regards,

Keita

Labels (6)
0 Kudos
Reply
1 Solution
1,011 Views
art
NXP Employee
NXP Employee

Yes, you are right, only Pro codec exists, and it already includes all Std features.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,012 Views
art
NXP Employee
NXP Employee

Yes, you are right, only Pro codec exists, and it already includes all Std features.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,011 Views
keitanagashima
Senior Contributor I

Dear Al,

Anyone, please follow my question.

Best Regards,

Keita

0 Kudos
Reply
1,011 Views
keitanagashima
Senior Contributor I

Dear All,

Hello.

Do you have any update?

Best Regards,

Keita

0 Kudos
Reply