About WMA10 Std decoder in KK4.4.3_2.0.0 with i.MX6DQ.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About WMA10 Std decoder in KK4.4.3_2.0.0 with i.MX6DQ.

跳至解决方案
1,188 次查看
keitanagashima
Senior Contributor I

Dear All,

Hello. 

Refer to 5.4 Audio decoder in "i.MX Android Extended Codec Release Note" of Rev KK4.4.3_2.0.0-ga.

There is description of "WMA10 Std".

But, we think that "WMA10 Std" doesn't exist. (Only existing the WMA10 Pro.)

Does "WMA10 Std" exist?

Best Regards,

Keita

标签 (6)
0 项奖励
回复
1 解答
1,009 次查看
art
NXP Employee
NXP Employee

Yes, you are right, only Pro codec exists, and it already includes all Std features.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,010 次查看
art
NXP Employee
NXP Employee

Yes, you are right, only Pro codec exists, and it already includes all Std features.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,009 次查看
keitanagashima
Senior Contributor I

Dear Al,

Anyone, please follow my question.

Best Regards,

Keita

0 项奖励
回复
1,009 次查看
keitanagashima
Senior Contributor I

Dear All,

Hello.

Do you have any update?

Best Regards,

Keita

0 项奖励
回复