About VDD_SNVS_IN voltage spec. of i.MX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About VDD_SNVS_IN voltage spec. of i.MX6UL

跳至解决方案
1,085 次查看
yuuki
Senior Contributor II

Dear all,

We look at the data sheet of i.MX6UL.

According to Table 8, Absolute Maximum Rating of VDD_SNVS_IN is -0.3V to 3.4V.

MX6UL_Absolute_Maximum_Ratings.png

However, VDD_SNVS_IN's Operating Range is 2.4V to 3.6V.

MX6UL_Operating_Ranges.png

For Max value, Absolute Maximum Rating < Operating Range

We think that a value of Absolute Maximum Rating is mistake.

Would you tell me the correct value of Absolute Maximum Rating?

Best Regards,

Yuuki

标签 (1)
0 项奖励
回复
1 解答
654 次查看
Yuri
NXP Employee
NXP Employee

Hello,

"Design team confirm it should be:
Operation Rating, VDD_SNVS_IN: 2.4 ~ 3.6V
Absolute Maximum Ratings, VDD_SNVS_IN: -0.3 ~ 3.6V

And we will modify the datasheet in next release".

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
655 次查看
Yuri
NXP Employee
NXP Employee

Hello,

"Design team confirm it should be:
Operation Rating, VDD_SNVS_IN: 2.4 ~ 3.6V
Absolute Maximum Ratings, VDD_SNVS_IN: -0.3 ~ 3.6V

And we will modify the datasheet in next release".

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复