About VDD_SNVS_IN voltage spec. of i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About VDD_SNVS_IN voltage spec. of i.MX6UL

Jump to solution
1,190 Views
yuuki
Senior Contributor II

Dear all,

We look at the data sheet of i.MX6UL.

According to Table 8, Absolute Maximum Rating of VDD_SNVS_IN is -0.3V to 3.4V.

MX6UL_Absolute_Maximum_Ratings.png

However, VDD_SNVS_IN's Operating Range is 2.4V to 3.6V.

MX6UL_Operating_Ranges.png

For Max value, Absolute Maximum Rating < Operating Range

We think that a value of Absolute Maximum Rating is mistake.

Would you tell me the correct value of Absolute Maximum Rating?

Best Regards,

Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
759 Views
Yuri
NXP Employee
NXP Employee

Hello,

"Design team confirm it should be:
Operation Rating, VDD_SNVS_IN: 2.4 ~ 3.6V
Absolute Maximum Ratings, VDD_SNVS_IN: -0.3 ~ 3.6V

And we will modify the datasheet in next release".

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
760 Views
Yuri
NXP Employee
NXP Employee

Hello,

"Design team confirm it should be:
Operation Rating, VDD_SNVS_IN: 2.4 ~ 3.6V
Absolute Maximum Ratings, VDD_SNVS_IN: -0.3 ~ 3.6V

And we will modify the datasheet in next release".

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply