Hello,community
About TDSR time in Figure 13-14 of i.MX 7Dual Applications Processor Reference Manual
The low time of the RD signal on the LCD side is min355ns.
Is the TDSR time the same as DISPLAY CLOCK (pix_clk)?
What equation should be used to calculate the value of which register to set TDSR to 2.8MHz (1 / 355ns)?
Best Regards,
Goto
Solved! Go to Solution.
Hello,
The timing parameters TCS, TCH, TDSR and TDHR are programmable. Use LCD Interface
Timing Register (LCDIFx_TIMING) and “Code Example to Initialize the eLCDIF in MPU Write Mode”
chapter in the RM. The timing values are set as number of DISPLAY CLOCK (pix_clk) cycles.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
Hello,
The timing parameters TCS, TCH, TDSR and TDHR are programmable. Use LCD Interface
Timing Register (LCDIFx_TIMING) and “Code Example to Initialize the eLCDIF in MPU Write Mode”
chapter in the RM. The timing values are set as number of DISPLAY CLOCK (pix_clk) cycles.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.