About Stopping the CSI_PIXCLK of Gated Clock Mode Timing in i.MX6SL.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Stopping the CSI_PIXCLK of Gated Clock Mode Timing in i.MX6SL.

Jump to solution
636 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.I have a question about CSI_PIXCLK of Gated Clock Mode Timing in i.MX6SL.

Refer to "4.10.2.0.1 Gated Clock Mode Timing" in IMX6SLCEC_Rev.3.

There is below description.

"The pixel clock, CSI_PIXCLK (PIXCLK), is valid as long as HSYNC is asserted."

Is it possible to stop CSI_PIXCLK (PIXCLK) from external device, as long as HSYNC is de-asserted?

Best Regards,

Keita

Labels (1)
0 Kudos
Reply
1 Solution
515 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes possible. Timing is similar to non-gated mode, RM shows it :

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
516 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes possible. Timing is similar to non-gated mode, RM shows it :

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply