About OMX Player in AndroidM6.0.1_2.1.0 for i.MX6Q-SABRE-SDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About OMX Player in AndroidM6.0.1_2.1.0 for i.MX6Q-SABRE-SDB

779件の閲覧回数
yuuki
Senior Contributor II

Daer all,

We run AndroidM6.0.1_2.1.0 BSP on i.MX6Quad SABRE-SDB.

According to the following release note, Stagefright is used as default media framework.
And the OMXPlayer is only used for RTP/UDP streaming.

- i.MX_Android_Extended_Codec_Release_Notes.pdf

The OMXPlayer was used in Android4 .4.3.

We want to use by default OMXPlayer on AndroidM6.0.1_2 .1.0.

Can we use by default OMXPlayer?
Would you tell me the method if it is possible?

Best Regards,
Yuuki

ラベル(2)
0 件の賞賛
3 返答(返信)

528件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi yuuki,

Codecs that have license restriction are provided in separate packages.For Install the OMXPlayer as default media framework you need to get the sources packages and rebuild the bsp. To obtain the mentioned package, you should contact with Freescale local FAE or Marketing office.

Regards

 

0 件の賞賛

528件の閲覧回数
yuuki
Senior Contributor II

Dear Bio_TICFSL-san,

AndroidKK4 .4.3 needed OMXPlayer package.

However, we understand that AndroidM6.0.1_2 .1.0 has already included OMXPlayer.
"Used Stagefright as the default media framework rather than OMXPlayer. OMXPlayer is only used for RTP/UDP streaming."

Is my understanding wrong?
Does OMX player package for AndroidM6.0.1_2 .1.0 exist separately?

Best Regards,
Yuuki

0 件の賞賛

528件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Yuuki,

Correct!, M6.0.1_2.1.0 does not provide source of omxplayer/wfdsink separately, all source is included in one package. and need to be provided via Marketing.

Regards

0 件の賞賛