About DDR Test Tool(i.MX7D)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About DDR Test Tool(i.MX7D)

Jump to solution
1,349 Views
goto11
Contributor III

Hello,Community

Decompressed ddr_stress_tester_v3.00_setup.exe and tried to carry out calibration of LPDDR3.
DDR frequency of 533MHz could not be tested.
ERROR : Calibration freq you entered is out of range (300 ~ 528MHz)!

On the other hand, the following is described in 1.4.7 External Memory Interface of i.MX 7Dual Applications Processor Reference Manual.
• 32-bit LP-DDR3 up to 533MHz clock (1066MT / s)

Can I calibrate LPDDR3 at 533MHz?
Or is the Tool version old?

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
1,183 Views
Yuri
NXP Employee
NXP Employee

Hello,

  the restriction of 528 MHz is from tools, supporting i.MX6. I already reported about it to 

the team, but, at least till now this issue takes place. Note, hardly results for 528 MHz calibration

are significantly differ from ones of 533 MHz. 

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
3 Replies
1,183 Views
goto11
Contributor III

Hello,

Thank you for the information on i.MX7D DRAM Register Programming Aid.

Please let me know if you can calibrate LPDDR3 at 533MHz.

best regards

Goto

0 Kudos
Reply
1,184 Views
Yuri
NXP Employee
NXP Employee

Hello,

  the restriction of 528 MHz is from tools, supporting i.MX6. I already reported about it to 

the team, but, at least till now this issue takes place. Note, hardly results for 528 MHz calibration

are significantly differ from ones of 533 MHz. 

Regards,

Yuri.

0 Kudos
Reply
1,183 Views
Yuri
NXP Employee
NXP Employee

 

Hello,

 

  Use https://community.nxp.com/docs/DOC-152468  

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply