About BCLK toggle with synchronous access in i.MX6DQ.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About BCLK toggle with synchronous access in i.MX6DQ.

跳至解决方案
604 次查看
keitanagashima
Senior Contributor I

Dear All,

I have a question about BCLK toggles with synchronous access in i.MX6DQ.

Refer to Page.1019 in IMX6DQRM(Rev.2).

====

The BCLK signal toggles only when burst access is executed toward the external device (BCM=1'b0 for normal mode use).

====

We assume the single read / write and burst transfer with sync access (BCM=0).

In case of single read / write, does BCLK signal toggle (output)?

Best Regards,

Keita

标签 (5)
0 项奖励
回复
1 解答
510 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

BCM.jpg

>We assume the single read / write and burst transfer with sync access (BCM=0).

>In case of single read / write, does BCLK signal toggle (output)?

yes, at synchronous access BCLK signal toggles even in case of single

beat burst.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
511 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

BCM.jpg

>We assume the single read / write and burst transfer with sync access (BCM=0).

>In case of single read / write, does BCLK signal toggle (output)?

yes, at synchronous access BCLK signal toggles even in case of single

beat burst.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复